This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FPGA接DM8147 VIP0的portA 16bit discreate模式capture_link无法接收到数据



DM8147 VIP0的portA接FPGA无法接收到数据。

我们使用FPGA接4个AP0101,把四个数据通过FPGA合成一个之后通过VIP0的portA传给DM8147的HDVPSS,我们将ISS的初始化代码注释了,但是现在capturelink一直采集不到数据,请大神帮忙分析一下原因。

开发包IPNC_RDK3.5

现在我们用FPGA输出YUV数据,使用16根数据线,输入格式为SYSTEM_DF_YUV422P    SYSTEM_STD_1080P_30 使用CLK HSYNC 

以下是对程序的修改:

【ipnc_rdk中修改的内容】

文件captureLink_drv.c

Int32 CaptureLink_drvCreateInst(CaptureLink_Obj * pObj, UInt16 instId)
{
。。。

pVipCreateArgs->videoCaptureMode = VPS_CAPT_VIDEO_CAPTURE_MODE_SINGLE_CH_NON_MUX_DISCRETE_SYNC_HSYNC_VSYNC;
pVipCreateArgs->videoIfMode = VPS_CAPT_VIDEO_IF_MODE_16BIT;

。。。
}

并将system_m3vpss.c文件中Int32 System_init()中有关iss的代码都注释掉

【HDVPSS中修改的内容】

文件:vpsdrv_captureVip.c中修改的内容(函数Vps_captVipParserConfigSetup中)

vipPortConfig->disConfig.fidDetectMode = VPS_VIP_FID_DETECT_MODE_VSYNC;//zzh
vipPortConfig->disConfig.actvidPol = VPS_VIP_POLARITY_HIGH;
vipPortConfig->disConfig.vsyncPol = VPS_VIP_POLARITY_HIGH;
vipPortConfig->disConfig.hsyncPol = VPS_VIP_POLARITY_HIGH;



usecase:

CaptureLink_CreateParams_Init(&capturePrm);
capturePrm.numVipInst = 1; //1个采集口
//capturePrm.outQueParams[0].nextLink = nNullID;
capturePrm.outQueParams[0].nextLink = gVencModuleContext.ipcM3OutId;//gVcapModuleContext.nsfId[0];// gMultiCh_VsrcVencObj.ipcOutVpssId;////下一个linkID
capturePrm.tilerEnable = FALSE; //停用tiler
capturePrm.fakeHdMode = FALSE; //是否启用模拟1080P输出
capturePrm.enableSdCrop = FALSE; //是否启用裁剪 采集为D1时有用 将720裁剪为704
capturePrm.doCropInCapture = FALSE; //是否启用裁剪 采集为D1时有用 将720裁剪为704 通过调整指针的方式实现 //采集通道参数设置
for(vipInstId=0; vipInstId<capturePrm.numVipInst; vipInstId++)
{
pCaptureInstPrm = &capturePrm.vipInst[vipInstId];
pCaptureInstPrm->vipInstId = (SYSTEM_CAPTURE_INST_VIP0_PORTA+vipInstId)%SYSTEM_CAPTURE_INST_MAX;/*ID设置*/
pCaptureInstPrm->videoDecoderId = 0; /* Need to change based on actual HD video decoder */
pCaptureInstPrm->inDataFormat = SYSTEM_DF_YUV422P;//SYSTEM_DF_YUV422I_YUYV;
//pCaptureInstPrm->standard = SYSTEM_STD_1944P_14;
pCaptureInstPrm->standard = SYSTEM_STD_1080P_30; /* Need to change based on actual HD video decoder */
pCaptureInstPrm->numOutput = 1; /* Need to change based on actual HD video decoder */

pCaptureOutPrm = &pCaptureInstPrm->outParams[0];
pCaptureOutPrm->dataFormat = SYSTEM_DF_YUV420SP_UV;//SYSTEM_DF_YUV420SP_UV;//
pCaptureOutPrm->scEnable = FALSE; /* Need to change based on actual HD video decoder */
pCaptureOutPrm->scOutWidth = 1920; /* Need to change based on actual HD video decoder */
pCaptureOutPrm->scOutHeight = 1080; /* Need to change based on actual HD video decoder */
pCaptureOutPrm->outQueId = 0;
}

设备启动时的打印信息

********** FULL FEATURE USECASE ********

[host] ********* Entered MultiCh_createTriStreamFullFtr ********


[host] 143: MCFW : CPU Revision [ES2.1] !!!

[host] 144: MCFW : Detected [UNKNOWN] Board !!!

[host] 144: MCFW : Base Board Revision [REV A] !!!
[m3vpss ] VPS_DCTRL_INST_0
[m3vpss ] IOCTL_VPS_DCTRL_SET_VENC_OUTPUT SYSTEM_DC_VENC_DVO2
[m3vpss ] IOCTL_VPS_DCTRL_SET_VENC_OUTPUT SYSTEM_DC_VENC_HDMI
[m3vpss ] IOCTL_VPS_DCTRL_SET_VENC_OUTPUT SYSTEM_DC_VENC_SD
[m3vpss ] IOCTL_VPS_DCTRL_SET_VENC_CLK_SRC VPS_DC_VENC_HDMI | VPS_DC_VENC_DVO2
[m3vpss ] 11676: CAPTURE: Create in progress !!!
[m3vpss ] Vps_captCreate ## start ...
[m3vpss ] ################## pInstPrm->standard : default
[m3vpss ] 11714: CAPTURE: VIP0 PortA capture mode is [16-bit, Non-mux Discrete Sync - ACTVID_VSYNC] !!!
[m3vpss ] Vps_captCreate ## start ...
[m3vpss ] Vps_captCreate ## 1
[m3vpss ] Vps_captCreate ## 2
[m3vpss ] Vps_captCreate ## 3
[m3vpss ] Vps_captCreate ## 4
[m3vpss ] Vps_captCreate ## 5
[m3vpss ] Vps_captCreate ## 6
[m3vpss ] Vps_captCreate ## 7
[m3vpss ] Vcore_vipResAllocPath ### input source is single-channel YUV422 ...
[m3vpss ] Vps_captCreateChObj ## VPDMA CH ID vChannelId[0]:104
[m3vpss ] Vps_captCreateChObj ## VPDMA CH ID vChannelId[1]:105
[m3vpss ] Vps_captCreate ## 7 - 1
[m3vpss ] ----------------------------------------------------
[m3vpss ] drivers/capture/src/vpsdrv_captureVip.c:334
[m3vpss ] vipInstConfig->intfMode : 1
[m3vpss ] vipInstConfig->vipConfig.clipActive : 0
[m3vpss ] vipInstConfig->vipConfig.clipBlank : 0
[m3vpss ] ----------------------------------------------------
[m3vpss ] vipPortConfig->syncType : 4
[m3vpss ] vipPortConfig->ctrlChanSel : 1
[m3vpss ] vipPortConfig->ancChSel8b : 0
[m3vpss ] vipPortConfig->pixClkEdgePol : 0
[m3vpss ] vipPortConfig->invertFidPol : 0
[m3vpss ] vipPortConfig->invertFidPol : 0
[m3vpss ] vipPortConfig->enablePort : 1
[m3vpss ] vipPortConfig->clrAsyncFifoRd : 0
[m3vpss ] vipPortConfig->clrAsyncFifoWr : 0
[m3vpss ] vipPortConfig->discreteBasicMode : 1
[m3vpss ] ----------------------------------------------------
[m3vpss ] vipPortConfig->disConfig.fidSkewPostCnt : 0
[m3vpss ] vipPortConfig->disConfig.fidSkewPreCnt : 0
[m3vpss ] vipPortConfig->disConfig.lineCaptureStyle : 1
[m3vpss ] vipPortConfig->disConfig.fidDetectMode : 1
[m3vpss ] vipPortConfig->disConfig.actvidPol : 1
[m3vpss ] vipPortConfig->disConfig.vsyncPol : 1
[m3vpss ] vipPortConfig->disConfig.hsyncPol : 1
[m3vpss ] ----------------------------------------------------
[m3vpss ] Vps_captCreate ## 7 - 2
[m3vpss ] Vps_captCreate ## 7 - 3
[m3vpss ] Vps_captCreate ## 7 - 4
[m3vpss ] Vps_captCreate ## 7 - 5
[m3vpss ] Vps_captCreate ## 7 - 6
[m3vpss ] Vps_captCreate ## 7 - 7
[m3vpss ] Vps_captCreate ## 7 - 8
[m3vpss ] Vps_captCreate ## 8
[m3vpss ] Disable VIP cropping ## 393:Vps_captCreate
[m3vpss ] Vps_captCreate ## end ...

[host] IpcBitsInLink_tskMain:Entered
[host] 556: IPC_BITS_IN : Create in progress !!!

[host] 556: IPC_BITS_IN : ListMPOpen start !!!

[host] 556: SYSTEM: Opening ListMP [VIDEO-M3_IPC_OUT_28] ...
[m3video] 11974: IPC_IN_M3 : Create in progress !!!
[m3video] 11974: SYSTEM: Opening ListMP [VPSS-M3_IPC_OUT_0] ...
[m3video] 11975: SYSTEM: Opening ListMP [VPSS-M3_IPC_IN_0] ...
[m3vpss ] CAPTURE::HEAPID:0 USED:192
[m3video] 11978: IPC_IN_M3 : Create Done !!!
[m3vpss ] 11970: CAPTURE: Create Done !!!
[m3video] 11978: ENCODE: Create in progress ... !!!
[m3vpss ] 11971: IPC_OUT_M3 : Create in progress !!!
[m3video] 12007: ENCODE: Creating CH0 of 1920 x 1080, pitch = (1920, 1920) [PROGRESSIVE] [NON-TILED ], bitrate = 8000 Kbps ...
[m3vpss ] numCh: 0,frameSkipCtx.inputFrameRate: 30,frameSkipCtx.outputFrameRate:30
[m3vpss ] bufType = 0
[m3vpss ] codingformat = 0
[m3video] ENCLINK_H264:HEAPID:0 USED:13808
[m3vpss ] dataFormat = 7
[m3video] 12071: ENCODE: All CH Create ... DONE !!!
[m3vpss ] memType = 0
[m3vpss ] startX = 0
[m3vpss ] startY = 0
[m3video] ENCLINK:HEAPID:0 USED:14048
[m3vpss ] width = 1920
[m3video] 12074: ENCODE: Create ... DONE !!!
[m3vpss ] height = 1080
[m3video] 12074: IPC_BITS_OUT : Create in progress !!!
[m3vpss ] pitch[0] = 1920
[m3vpss ] pitch[1] = 1920
[m3vpss ] pitch[2] = 0
[m3video] 12077: IPC_BITS_OUT : Create Done !!!
[m3vpss ] scanFormat = 1
[m3vpss ] 11973: IPC_OUT_M3 : Create Done !!!

  • Liu Jiang,

    请问你是否有测量过FPGA输出时钟,同步信号是否正常?你是否有修改过时钟,同步信号的极性,看是否有帮助?

  • 谢谢您的回复!

    我们测试了FPGA的数据,FPGA 时钟为74.25MHz 使用CLK VSYNC HSYNC D[0-15]信号线,VSYNC和HSYNC都为高时数据有效。输出的视频为1920*1080 30帧

    现在找到之前采集不到数据的原因了: 我在Vps_captIsrListComplete()回调函数中添加了打印信息。去掉之后就有数据了。

    --------------------------------------------------------------------------------------------------------------------------------------

    回到函数所在文件vpsdrv_captureList.c

    /* Driver callback called by CLM with timer expires */
    Void Vps_captIsrListComplete()
    {
    /* get current time */
    gVps_captCommonObj.clockTicks = Clock_getTicks();

    ##########################去除的打印##############################
    // Vps_printf ( " %s:%d: Driver callback called by CLM with timer expires !!!\n",
    // __FUNCTION__, __LINE__);

    ##########################去除的打印##############################

    /* trigger list processing task */
    Semaphore_post(gVps_captCommonObj.semListUpdate);
    }

    --------------------------------------------------------------------------------------------------------------------------------------

    但是我们有遇到两个新的问题:

    1.captureLink采集的过程中会出现数据帧中的pFrame->reserved>0的问题,所以程序一直提示【[m3vpss ] 247926: CAPTURE: Dequeued frame more than once (0,0, b90f6e80)】。我们跟踪了一下代码发现好像是video 中H264压缩部分将pFrame->reserved设置为了当前时间,这个该如何解决啊?

    2.第二个问题是,如果设备上电FPGA在HDVPSS初始化之前就给数据信号的话,也会没有采集。我们将FPGA中加了100秒的延迟,在HDVPSS初始化完成之后FPGA再给数据信号(时钟信号一直在给)就能够正常采集。这可能是什么原因导致的?

    问题1的错误提示在文件 captureLink_drc.c 中的CaptureLink_drvProcessData函数

    Int32 CaptureLink_drvProcessData(CaptureLink_Obj * pObj)
    {
                        ...

                       tmpValue = (UInt32) pFrame->reserved;
                       if (tmpValue > 0)
                       {
                                Vps_printf
                                         (" %d: CAPTURE: Dequeued frame more than once (%d,%d, %08x) \n",
                                         Utils_getCurTimeInMsec(), queId, queChId, pFrame->addr[0][0]);
                       }
                      tmpValue++;
                      pFrame->reserved = (Ptr) tmpValue;

                     ...

    }

    问题1的错误提示:


    [m3vpss ] 247926: CAPTURE: Dequeued frame more than once (0,0, b90f6e80)
    [m3vpss ] 247966: CAPTURE: Dequeued frame more than once (0,0, b93ee480)
    [m3vpss ] 247998: CAPTURE: Dequeued frame more than once (0,0, b96e5a80)
    [m3vpss ] 248030: CAPTURE: Dequeued frame more than once (0,0, b99dd080)
    [m3vpss ] 248062: CAPTURE: Dequeued frame more than once (0,0, b9cd4680)
    [m3vpss ] 248094: CAPTURE: Dequeued frame more than once (0,0, b9fcbc80)
    [m3vpss ] 248126: CAPTURE: Dequeued frame more than once (0,0, ba2c3280)
    [m3vpss ] 248166: CAPTURE: Dequeued frame more than once (0,0, ba5ba880)
    [m3vpss ] 248198: CAPTURE: Dequeued frame more than once (0,0, ba8b1e80)
    [m3vpss ] 248230: CAPTURE: Dequeued frame more than once (0,0, b8810c80)
    [m3vpss ] 248262: CAPTURE: Dequeued frame more than once (0,0, b8b08280)
    [m3vpss ] 248294: CAPTURE: Dequeued frame more than once (0,0, b8dff880)
    [m3vpss ] 248326: CAPTURE: Dequeued frame more than once (0,0, b90f6e80)
    [m3vpss ] 248366: CAPTURE: Dequeued frame more than once (0,0, b93ee480)
    [m3vpss ] 248398: CAPTURE: Dequeued frame more than once (0,0, b96e5a80)
    [m3vpss ] 248430: CAPTURE: Dequeued frame more than once (0,0, b99dd080)
    [m3vpss ] 248462: CAPTURE: Dequeued frame more than once (0,0, b9cd4680)
    [m3vpss ] 248494: CAPTURE: Dequeued frame more than once (0,0, b9fcbc80)
    [m3vpss ] 248526: CAPTURE: Dequeued frame more than once (0,0, ba2c3280)
    [m3vpss ] 248566: CAPTURE: Dequeued frame more than once (0,0, ba5ba880)
    [m3vpss ] 248598: CAPTURE: Dequeued frame more than once (0,0, ba8b1e80)
    [m3vpss ] 248630: CAPTURE: Dequeued frame more than once (0,0, b8810c80)
    [m3vpss ] 248662: CAPTURE: Dequeued frame more than once (0,0, b8b08280)
    [m3vpss ] 248694: CAPTURE: Dequeued frame more than once (0,0, b8dff880)
    [m3vpss ] 248726: CAPTURE: Dequeued frame more than once (0,0, b90f6e80)
    [m3vpss ] 248766: CAPTURE: Dequeued frame more than once (0,0, b93ee480)

  • 针对之前的问题2我们使用CCS查看了vin的寄存器值

    FPGA有延迟时,HDVPSS初始化之后FPGA再给数据信号。可以正常采集。

    FPGA没有延迟时,上电之后HDVPSS初始化之前就给数据信号,出现如图中的寄存器不同,提示output FIFO PortA Luma Overflow。我们在设备程序启动之后添加了调用采集部分重启的命令IOCTL_VPS_CAPT_RESET_AND_RESTART还是不行。这个问题该如何解决呢?

  • jiang liu4 说:
    1.captureLink采集的过程中会出现数据帧中的pFrame->reserved>0的问题,所以程序一直提示【[m3vpss ] 247926: CAPTURE: Dequeued frame more than once (0,0, b90f6e80)】。我们跟踪了一下代码发现好像是video 中H264压缩部分将pFrame->reserved设置为了当前时间,这个该如何解决啊?

    你好;

            你的fpga的输出是按照cea-861,参考标准时序输出的吗?

            你可以试一下修改采集模式:

    pVipCreateArgs->videoCaptureMode =
    VPS_CAPT_VIDEO_CAPTURE_MODE_SINGLE_CH_NON_MUX_DISCRETE_SYNC_ACTVID_VSYNC;

  • jiang liu4 说:
    2.第二个问题是,如果设备上电FPGA在HDVPSS初始化之前就给数据信号的话,也会没有采集。我们将FPGA中加了100秒的延迟,在HDVPSS初始化完成之后FPGA再给数据信号(时钟信号一直在给)就能够正常采集。这可能是什么原因导致的?

    正常应当是不会有这个问题的;

    即使fpga那边一直在输出数据,dm8147的这边的采集应当是没有问题的;

    你们怎么会选择IPNC RDK3.5的开发包,不使用DVRRDK的开发包直接开发呢;

  • 1. 我们买的开发板带的是IPNC RDK3.5的开发包,当时担心使用DVRRDK需要修改很多东西。我们是不是使用DVRRDK更合适。

    2.我们现在的程序配置是:

    pVipCreateArgs->videoCaptureMode = VPS_CAPT_VIDEO_CAPTURE_MODE_SINGLE_CH_NON_MUX_DISCRETE_SYNC_ACTVID_VBLK;
    pVipCreateArgs->videoIfMode = VPS_CAPT_VIDEO_IF_MODE_16BIT;


    vipPortConfig->disConfig.fidDetectMode = VPS_VIP_FID_DETECT_MODE_VSYNC;
    vipPortConfig->disConfig.actvidPol = VPS_VIP_POLARITY_HIGH;
    vipPortConfig->disConfig.vsyncPol = VPS_VIP_POLARITY_LOW;
    vipPortConfig->disConfig.hsyncPol = VPS_VIP_POLARITY_LOW;

    FPGA输出的信号

    FPGA的lv和fv为高的时候数据有效,现在我们让FPGA给的测试数据Y和UV数据给的是一样的,并且把FPGA的延迟取消了。

    现在设备上电之后,有时候capture能采集到数据,但多试几次就不行。

    CCS连接上设备查看寄存器,不出视频的时候中断状态寄存器中OUTPUT_FIFO_PRTA_LUMA_STATUS为1,文档中这一位解释为Output FIFO Port A luma Overflow Status

    当能够正常出视频时,连接上设备查看OUTPUT_FIFO_PRTA_LUMA_STATUS为0

  • 在之前的基础上又设置了下面两个选项并增加了VIP Overflow Recovery后能够正常的出图了,FPGA也不用延迟了。

    pObj->enableCheckOverflowDetect = TRUE;
    pVipCreateArgs->periodicCallbackEnable = TRUE;

    并且在Void App_runDemo(Void)函数最后又添加了VIP Overflow Recovery步骤,具体流程在文档 [HDVPSS User's Guide 1.2.8.2.19 VIP Overflow Detection and Recovery]

    现在我们将FPGA输出的分辨率修改为4096*960 30帧,时钟是150MHz。能够出图但是图像中从3840往后的uv数据不对,Y数据都是对的。请问DM8147的HDVPSS可以出4096*960 30帧的数据吗,现在我们只修改了capturelink创建时的分辨率,并将数据分辨率设置为了4096*960,这样修改对吗?

  • jiang liu4 说:
    能够出图但是图像中从3840往后的uv数据不对,

    请参考论坛讨论:http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/110471.aspx。

  • 谢谢您的回复

    我们将link修改了一样,在capturelink接了nsf,capturelink中不在做YUV转换,在nsf中做YUV转换现在可以出4096*960的分辨率了。

    /*capturePrm 参数设置*/
    CaptureLink_CreateParams_Init(&capturePrm);
    capturePrm.numVipInst = 1; //1个采集口
    capturePrm.outQueParams[0].nextLink = gVcapModuleContext.nsfId[0];//gVcapModuleContext.nsfId[0];// gMultiCh_VsrcVencObj.ipcOutVpssId;////下一个linkID
    capturePrm.tilerEnable = FALSE; //停用tiler
    capturePrm.fakeHdMode = FALSE; //是否启用模拟1080P输出
    capturePrm.enableSdCrop = FALSE; //是否启用裁剪 采集为D1时有用 将720裁剪为704
    capturePrm.doCropInCapture = FALSE; //是否启用裁剪 采集为D1时有用 将720裁剪为704 通过调整指针的方式实现 //采集通道参数设置
    for(vipInstId=0; vipInstId<capturePrm.numVipInst; vipInstId++)
    {
                  pCaptureInstPrm = &capturePrm.vipInst[vipInstId];
                 pCaptureInstPrm->vipInstId = (SYSTEM_CAPTURE_INST_VIP0_PORTA+vipInstId)%SYSTEM_CAPTURE_INST_MAX;/*ID设置*/
                 pCaptureInstPrm->videoDecoderId = 0; /* Need to change based on actual HD video decoder */
                 pCaptureInstPrm->inDataFormat = SYSTEM_DF_YUV422P;//SYSTEM_DF_YUV422I_YUYV;
                 pCaptureInstPrm->standard = SYSTEM_STD_AUTO_DETECT; /* Need to change based on actual HD video decoder */
                 pCaptureInstPrm->numOutput = 1; /* Need to change based on actual HD video decoder */

                 pCaptureOutPrm = &pCaptureInstPrm->outParams[0];
                 pCaptureOutPrm->dataFormat = SYSTEM_DF_YUV422I_YUYV;//SYSTEM_DF_YUV420SP_UV;//
                 pCaptureOutPrm->scEnable = FALSE; /* Need to change based on actual HD video decoder */
                 pCaptureOutPrm->scOutWidth = 4096; /* Need to change based on actual HD video decoder */
                 pCaptureOutPrm->scOutHeight = 960; /* Need to change based on actual HD video decoder */
                 pCaptureOutPrm->outQueId = 0;
    }

    NsfLink_CreateParams_Init(&nsfPrm);
    nsfPrm.bypassNsf = FALSE;
    nsfPrm.tilerEnable = FALSE;
    nsfPrm.inQueParams.prevLinkId = gVcapModuleContext.captureId;
    nsfPrm.inQueParams.prevLinkQueId = 0;
    nsfPrm.numOutQue = 1;
    nsfPrm.outQueParams[0].nextLink = gVencModuleContext.ipcM3OutId;