大家好,
最近在开发linux下的PCI驱动,6657作为EP,准备使用6657的EDMA来操作数据,
但是在MCSDK_2.1.2的linux_host_loader示例代码中只有6678的EDMA部分,我直接使用那部分代码来操作6657的EDMA,
程序会一直停留在 HAL_readDMA 或者 HAL_writeDMA , 应该是这个接口还没有适配 6657 , 所以想请教一下各位高手,
我该如何修改这个接口,才能在6657上正确使用。或者谁有相应的示例代码,那就更好了。
代码如下,在Hello World程序之后添加EDMA操作,程序会一直停留在 HAL_writeDMA接口
#if HELLO_WORLD_DEMO
/* Load DDR init code into DSP */
pushData(ddrInitCode, 0, &bootEntryAddr);
/* Write boot entry address into MAGIC_ADDR */
writeDSPMemory(0, MAGIC_ADDR, &bootEntryAddr, 4);
while (1) {
readDSPMemory(0, MAGIC_ADDR, buffer, 4);
if (buffer[0] == 0) break;
for (i = 0; i < 1000; i++) i++;
}
/* Load "Hello World" demo into DSP */
pushData(bootCode, 9, &bootEntryAddr);
/* Write boot entry address into MAGIC_ADDR */
writeDSPMemory(0, MAGIC_ADDR, &bootEntryAddr, 4);
#endif
printk("Allocating consistent memory ...\n");
wDataVirt = (uint8_t*)dma_alloc_coherent(&PCIE_DEV->dev, DMA_TRANSFER_SIZE, &wData, GFP_KERNEL);
rDataVirt = (uint8_t*)dma_alloc_coherent(&PCIE_DEV->dev, DMA_TRANSFER_SIZE, &rData, GFP_KERNEL);
for (i = 0; i < DMA_TRANSFER_SIZE; i++) {
wDataVirt[i] = i;
rDataVirt[i] = 0;
}
/* Wait 2 second for DDR init */
mdelay(2000);
printk ("Write DMA to DSP ...\n");
do_gettimeofday(&test_time1);
HAL_writeDMA (wData, DDR_START, DMA_TRANSFER_SIZE, 1); /* Move from GPP to DSP */
do_gettimeofday(&test_time2);
mdelay(1000);
printk("Read DMA from DSP ...\n");
do_gettimeofday(&test_time3);
HAL_readDMA(DDR_START, rData, DMA_TRANSFER_SIZE, 1); /* Move from DSP to GPP */
do_gettimeofday(&test_time4);
mdelay(1000);
/* For demo how to move inside DSP purpose only, you can directly move between GPP and DSP using flag = 1 */
// HAL_writeDMA (0x80000000, 0x11800000, 0x10000, 0);
// HAL_writeDMA (0x11800000, 0x0C000000, 0x10000, 0);
diff = (test_time2.tv_sec - test_time1.tv_sec)*1000000 + (test_time2.tv_usec - test_time1.tv_usec);
printk("DMA write throughput is: %d.%02d MB/s\n", DMA_TRANSFER_SIZE/(1024*1024)*1000*1000/diff,
((DMA_TRANSFER_SIZE/(1024*1024)*1000*1000)%diff)*100/diff);
diff = (test_time4.tv_sec - test_time3.tv_sec)*1000000 + (test_time4.tv_usec - test_time3.tv_usec);
printk("DMA read throughput is: %d.%02d MB/s\n", DMA_TRANSFER_SIZE/(1024*1024)*1000*1000/diff,
((DMA_TRANSFER_SIZE/(1024*1024)*1000*1000)%diff)*100/diff);
printk("Freeing consistent memory ...\n");
dma_free_coherent(&PCIE_DEV->dev, DMA_TRANSFER_SIZE, wDataVirt, wData);
dma_free_coherent(&PCIE_DEV->dev, DMA_TRANSFER_SIZE, rDataVirt, rData);