This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

要疯了! TI-processor- sdk -xxx-02.000.01.07 SD卡的官方大系统,跑QT5.5 的QTQucik 跑不起来



请教下:TI-processor- sdk -xxx-02.000.01.07    SD卡的官方大系统,跑qucik 跑不起来 。

例子里部分quick可以跑,自己写的不行,发现是用了QtQuick.Controls等的包都不行。

用SDK 提供的方法,source environment-setup 启动QT5.5的  qtceeator 

QML debugging is enabled. Only use this in a safe environment.
PVR: Hint: Setting WindowSystem to libpvrDRMWSEGL_FRONT.so

mode for connector 20 is 800x480
DRM SET CRTC: index: 0 fd: 6, crtc: 12, fb: 19, conn: 14, mode: 800x480
Unable to query physical screen size, defaulting to 100 dpi.
To override, set QT_QPA_EGLFS_PHYSICAL_WIDTH and QT_QPA_EGLFS_PHYSICAL_HEIGHT (in millimeters).
No such plugin for spec "Auto"
QQmlApplicationEngine failed to load component
qrc:/main.qml:3 module "QtQuick.Controls" is not installed

随便建立个例子,都跑不起。如图:

感觉就是少库了,不知道TI有没有我完整的编译了QT5.5的库。?好像QTQuick  下的很多库都找不到?是不是要自己重新搞下?