TI 工程师,你好:
我们的产品是基于DM8147开发的,之前使用的是4片 256M的DDR3,现在想去掉2片,将内存有1G的降为512M,我们在原来的开发板上去掉了2片DDR3,我们之前的ddr3使用的16位;每个bank有2片ddr3, 一起是32位,现在我们采取的是把每个bank的高16位去掉;
现在的问题是,通过防真器加载gel文件失败,问一下,像这样调整ddr,除了需要修改ddr3的相关配置寄存器值外,硬件上是不用做调整的吧?另外有没有类似的用例可以参考?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI 工程师,你好:
我们的产品是基于DM8147开发的,之前使用的是4片 256M的DDR3,现在想去掉2片,将内存有1G的降为512M,我们在原来的开发板上去掉了2片DDR3,我们之前的ddr3使用的16位;每个bank有2片ddr3, 一起是32位,现在我们采取的是把每个bank的高16位去掉;
现在的问题是,通过防真器加载gel文件失败,问一下,像这样调整ddr,除了需要修改ddr3的相关配置寄存器值外,硬件上是不用做调整的吧?另外有没有类似的用例可以参考?谢谢!
benyun zhu 说:需要修改ddr3的相关配置寄存器值
请问你们是修改了两个EMIF的位宽为16-bit么?
xiaoyan Chi 说:我们也是想从4片16bit,改为2片16bit,
请问你想用一个EMIF的32-bit,还是两个EMIF的两个低16-bit?
是不是用两个低16bit对速度影响小一些,只用一个EMIF会不会影响ddr速度
xiaoyan Chi 说:是不是用两个低16bit对速度影响小一些,只用一个EMIF会不会影响ddr速度
和2x32bit位宽来说,速率都大大减少了。
一个EMIF和两个EMIF的16-bit使用,如果使用interlace mode,差别不会太大。如果可以,建议用一个EMIF。
Chi Xiaoyan,
请参考数据手册里对于unused pin的要求。