This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

在vpss驱动手册中看到,如果DM8168程序通过HDMI与VGA都能显示,应该怎么做?



问1:在vpss驱动手册中看到,如果DM8168程序通过HDMI与VGA都能显示,应该怎么做?


通过
cat /sys/devices/platform/vpss/graphics0/nodes
cat /sys/devices/platform/vpss/graphics1/nodes
cat /sys/devices/platform/vpss/graphics2/nodes
看到默认
/dev/fb0 ---hdmi---------display0(Sysfs Name)
/dev/fb1 ---hdcomp-------display3(Sysfs Name)
/dev/fb2 ---sd-----------display2(Sysfs Name)

fb0 默认对应hdmi输出,fb1对应vga输出

VGA的电路引脚连线
AT9---RGB_HS
AP9---RGB_VS

AT21--IOUTA(R)
AR21--IOUTB(G)
AP21--IOUTC(B)

HDMI可以显示图像,为什么VGA没有图像显示呢?

谢谢!

另外如果想关闭的话,不能关闭display0,display1,display3,提示-sh: echo: write error: Invalid argument,请问为什么?

root@HDMTerm:~#
root@HDMTerm:~# echo 0 > /sys/devices/platform/vpss/display0/enabled
-sh: echo: write error: Invalid argument
root@HDMTerm:~# echo 0 > /sys/devices/platform/vpss/display1/enabled
-sh: echo: write error: Invalid argument
root@HDMTerm:~# echo 0 > /sys/devices/platform/vpss/display2/enabled
root@HDMTerm:~# echo 0 > /sys/devices/platform/vpss/display3/enabled
-sh: echo: write error: Invalid argument
root@HDMTerm:~# echo 1 > /sys/devices/platform/vpss/display1/enabled
root@HDMTerm:~# echo 1 > /sys/devices/platform/vpss/display2/enabled
root@HDMTerm:~# echo 1 > /sys/devices/platform/vpss/display3/enabled
root@HDMTerm:~# echo 1 > /sys/devices/platform/vpss/display0/enabled
root@HDMTerm:~# echo 1 > /sys/devices/platform/vpss/display4/enabled