This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Andy Yin1您好,感谢您的回答。我再cfg文件中只找到了Hwi的声明,并未对硬件中断的参数进行配置,在主函数中也只配置了Task的参数,是否代表Hwi只有声明但并未使用?
cfgScript代码如下:
var BIOS = xdc.useModule ("ti.sysbios.BIOS");
var Task = xdc.useModule ("ti.sysbios.knl.Task");
var ECM = xdc.useModule ("ti.sysbios.family.c64p.EventCombiner");
var C64_Hwi = xdc.useModule ("ti.sysbios.family.c64p.Hwi");
var Startup = xdc.useModule ("xdc.runtime.Startup");
var System = xdc.useModule ("xdc.runtime.System");
var Log = xdc.useModule ("xdc.runtime.Log");
var Hwi = xdc.useModule('ti.sysbios.hal.Hwi');
var Semaphore = xdc.useModule('ti.sysbios.knl.Semaphore');
var Cache = xdc.useModule('ti.sysbios.hal.Cache');
var CpIntc = xdc.useModule('ti.sysbios.family.c66.tci66xx.CpIntc');
ECM.eventGroupHwiNum[0] = 7;
ECM.eventGroupHwiNum[1] = 8;
ECM.eventGroupHwiNum[2] = 9;
ECM.eventGroupHwiNum[3] = 10;
/* Shared Memory base address and length */
var SHAREDMEM = 0x0C000000;
var SHAREDMEMSIZE = 0x00200000;
/*var SHAREDMEMSIZE = 0x00200000;*/
/*
* Since this is a single-image example, we don't (at build-time) which
* processor we're building for. We therefore supply 'null'
* as the local procName and allow IPC to set the local procId at runtime.
*/
var MultiProc = xdc.useModule('ti.sdo.utils.MultiProc');
MultiProc.setConfig(null, ["CORE0", "CORE1", "CORE2", "CORE3", "CORE4", "CORE5", "CORE6", "CORE7"]);
/*
* The SysStd System provider is a good one to use for debugging
* but does not have the best performance. Use xdc.runtime.SysMin
* for better performance.
*/
var System = xdc.useModule('xdc.runtime.System');
var SysStd = xdc.useModule('xdc.runtime.SysStd');
System.SupportProxy = SysStd;
/* Modules explicitly used in the application */
var MessageQ = xdc.useModule('ti.sdo.ipc.MessageQ');
var Ipc = xdc.useModule('ti.sdo.ipc.Ipc');
var HeapBufMP = xdc.useModule('ti.sdo.ipc.heaps.HeapBufMP');
var MultiProc = xdc.useModule('ti.sdo.utils.MultiProc');
/* BIOS/XDC modules */
var BIOS = xdc.useModule('ti.sysbios.BIOS');
BIOS.heapSize = 0x8000;
var Task = xdc.useModule('ti.sysbios.knl.Task');
/*var tsk0 = Task.create('&tsk0_func');*/
/*tsk0.instance.name = "tsk0";*/
/* Synchronize all processors (this will be done in Ipc_start) */
Ipc.procSync = Ipc.ProcSync_ALL;
/* enable fast message Q */
var MessageQ = xdc.module('ti.sdo.ipc.MessageQ');
var Notify = xdc.module('ti.sdo.ipc.Notify');
Notify.SetupProxy = xdc.module('ti.sdo.ipc.family.c647x.NotifyCircSetup');
MessageQ.SetupTransportProxy = xdc.module('ti.sdo.ipc.transports.TransportShmNotifySetup');
/* data section */
Program.sectMap[".internalMEM"]={runSegment: "L2SRAM_1"};
Program.sectMap[".externalMEM"]={runSegment: "DDR_1"};
Program.sectMap[".sharedMEM"]={runSegment: "MSMCSRAM_2"};
/*Program.sectMap[".internalL1SRAMMEM"]={runSegment: "L1SRAM"};*/
/*
* Need to define the shared region. The IPC modules use this
* to make portable pointers. All processors need to add this
* call with their base address of the shared memory region.
* If the processor cannot access the memory, do not add it.
*/
var SharedRegion = xdc.useModule('ti.sdo.ipc.SharedRegion');
SharedRegion.setEntryMeta(0,
{ base: SHAREDMEM,
len: SHAREDMEMSIZE,
ownerProcId: 0,
isValid: true,
name: "MSMC RAM",
});
/* Reset function initialize HW */
var Reset = xdc.useModule("xdc.runtime.Reset");
Reset.fxns[Reset.fxns.length++] = "&vlfft_system_reset";