我大概看了一下它们的引脚,感觉基本一样,尺寸也差不多,现在能不能用c6654的原理图和PCB封装代替c6655?文档里具体哪个地方有没有明确说明c6654的封装可以给c6655用?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
可以替代。下面是e2e上工程师的回复。
Yes, you can use the same PCB which was designed for C6655 to evaluate the C6654 device. The operating frequency is less in C6654 and some of the peripherals are not available. You can compare between the two devices using the functional block diagram in the device data manual.
另外,c6655属于多核,有专门的多核论坛支持。