This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

咨询6657的spi nor flash加载的ddr table



各位大神:

我的6657双核加载起来了 但没使用DDR TABLE

想咨询一下6657的DDR TABLE如何添加?
我看6657的文档 没有提到任何有关ddr configuration table的资料

难道6657不需要ddr configuration table 6678需要ddr configuration table???

文档没有有关说明:

/*******************************************************************************
* Emif4 (DDR3) configuration table
*******************************************************************************/
typedef struct bootEmif4Tbl_s {

UINT32 configSelect_msw; /* Bit map defining which registers to set */
UINT32 configSelect_slsw; /* Bit map defining which registers to set */
UINT32 configSelect_lsw; /* Bit map defining which registers to set */

UINT32 pllPrediv; /* Values of all 0s will disable the pll */
UINT32 pllMult;
UINT32 pllPostDiv;

UINT32 sdRamConfig; /* Controlled by bit 1 of configSelect_msw */
UINT32 sdRamConfig2; /* Bit 2 */
UINT32 sdRamRefreshCtl; /* Bit 3 */
UINT32 sdRamTiming1; /* Bit 4 */
UINT32 sdRamTiming2; /* Bit 5 */
UINT32 sdRamTiming3; /* Bit 6 */
UINT32 lpDdrNvmTiming; /* Bit 7 */
UINT32 powerManageCtl; /* Bit 8 */
UINT32 iODFTTestLogic; /* Bit 9 */
UINT32 performCountCfg; /* Bit 10 */
UINT32 performCountMstRegSel; /* Bit 11 */
UINT32 readIdleCtl; /* Bit 12 */
UINT32 sysVbusmIntEnSet; /* Bit 13 */
UINT32 sdRamOutImpdedCalCfg; /* Bit 14 */
UINT32 tempAlterCfg; /* Bit 15 */
UINT32 ddrPhyCtl1; /* Bit 16 */
UINT32 ddrPhyCtl2; /* Bit 17 */
UINT32 priClassSvceMap; /* Bit 18 */
UINT32 mstId2ClsSvce1Map; /* Bit 19 */
UINT32 mstId2ClsSvce2Map; /* Bit 20 */
UINT32 eccCtl; /* Bit 21 */
UINT32 eccRange1; /* Bit 22 */
UINT32 eccRange2; /* Bit 23 */
UINT32 rdWrtExcThresh; /* Bit 24 */

UINT32 chipConfig[64];

} BOOT_EMIF4_TBL_T;