This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am335x tlv320aic3106 无法录音

Other Parts Discussed in Thread: TLV320AIC3106, TPS65217

平台: am335x  tlv320aic3106 购买的开发板

kernel: linux-3.12.10

以前在linux3.2上面是没有问题的, 现在移植到3.12上面无法录音。 edma也已经注册。 不好意思 图传不上来

我只有文字描述了:

CPU           <----------------->  tlv320aic3106

外部12M 晶振      <---------->     MCLK

MCASP0_FSR. MCASP1_FSX  <--------> WCLK

MCASP0_ACLKR. MCASP1_ACLKX <--------> BCLK

MCASP0_AXR1, MCASP1_AXR0 <----------> DIN

MCASP0_AHCLKX. MCASP1_AXR1 <-------> DOUT

HPROUT-----------------------|      HEADPHONE

HPLOUT------------------------|

MICBIAS-   LINE2LP---------------------> MIC

LINE1LP  LINE1RP-----------> LINE IN

在3.2上面是在line in上面测试录音

arecord -d 10 -f cd -t wav  foobar.wav

在3.12上面 line in 和mic 都测试过  录音的时候不报错  用aplay播放 foobar.wav没有声音 同样不报错

mcasp1_pins: mcasp1_pins {
            pinctrl-single,pins = <
                0x1A4 (PIN_INPUT_PULLDOWN | MUX_MODE3) /* mii1_crs.mcasp1_aclkx */
                0x1A0 (PIN_INPUT_PULLDOWN | MUX_MODE3) /* mii1_rxerr.mcasp1_fsx */
                0x1A8 (PIN_OUTPUT_PULLDOWN | MUX_MODE3) /* mii1_col.mcasp1_axr2 */
                0x1AC (PIN_INPUT_PULLDOWN | MUX_MODE3) /* rmii1_ref_clk.mcasp1_axr3 */
            >;
        };

        mcasp1_sleep_pins: mcasp1_sleep_pins {
            pinctrl-single,pins = <
                0x1A4 (PIN_INPUT_PULLDOWN | MUX_MODE7)
                0x1A0 (PIN_INPUT_PULLDOWN | MUX_MODE7)
                0x1A8 (PIN_INPUT_PULLDOWN | MUX_MODE7)
                0x1AC (PIN_INPUT_PULLDOWN | MUX_MODE7)
            >;
        };

i2c1: i2c@4802a000 {
            pinctrl-names = "default";
            pinctrl-0 = <&i2c1_pins>;

            status = "okay";
            clock-frequency = <100000>;

            tlv320aic3106: tlv320aic3106@1b {
                compatible = "ti,tlv320aic3106";
                reg = <0x1b>;
                status = "okay";

                /* Regulators */
                AVDD-supply = <&ldo4_reg>;
                IOVDD-supply = <&ldo4_reg>;
                DRVDD-supply = <&ldo4_reg>;
                DVDD-supply = <&ldo3_reg>;
            };
        };

sound {
            compatible = "ti,da830-evm-audio";
            ti,model = "AM335x-EVM";
            ti,audio-codec = <&tlv320aic3106>;
            ti,mcasp-controller = <&mcasp1>;
            ti,codec-clock-rate = <12000000>;
            ti,audio-routing =
                "Headphone Jack",       "HPLOUT",
                "Headphone Jack",       "HPROUT",
                "LINE1L",               "Line In",
                "LINE1R",               "Line In";
        };

#include "tps65217.dtsi"

&mcasp1 {
        pinctrl-names = "default", "sleep";
        pinctrl-0 = <&mcasp1_pins>;
        pinctrl-1 = <&mcasp1_sleep_pins>;

        status = "okay";

        op-mode = <0>;          /* MCASP_IIS_MODE */
        tdm-slots = <2>;
        /* 16 serializer */
        serial-dir = <  /* 0: INACTIVE, 1: TX, 2: RX */
            1 2 0 0
        >;
        tx-num-evt = <32>;
        rx-num-evt = <32>;
};

&tps {
    regulators {
        dcdc1_reg: regulator@0 {
            /* +1.5V voltage with ±4% tolerance */
            regulator-min-microvolt = <900000>;
            regulator-max-microvolt = <1800000>;
            regulator-boot-on;
            regulator-always-on;
        };

        dcdc2_reg: regulator@1 {
            /* VDD_MPU voltage limits 0.95V - 1.1V with ±4% tolerance */
            regulator-name = "vdd_mpu";
            regulator-min-microvolt = <900000>;
            regulator-max-microvolt = <3300000>;
            regulator-boot-on;
            regulator-always-on;
        };

        dcdc3_reg: regulator@2 {
            /* VDD_CORE voltage limits 0.95V - 1.1V with ±4% tolerance */
            regulator-name = "vdd_core";
            regulator-min-microvolt = <900000>;
            regulator-max-microvolt = <1500000>;
            regulator-boot-on;
            regulator-always-on;
        };

        ldo1_reg: regulator@3 {
            /* +1.8V voltage with ±4% tolerance */
            regulator-min-microvolt = <1000000>;
            regulator-max-microvolt = <3300000>;
            regulator-boot-on;
            regulator-always-on;
        };

        ldo2_reg: regulator@4 {
            /* +3.3V voltage with ±4% tolerance */
            regulator-min-microvolt = <900000>;
            regulator-max-microvolt = <3300000>;
            regulator-boot-on;
            regulator-always-on;
        };

        ldo3_reg: regulator@5 {
            /* +1.8V voltage with ±4% tolerance */
            regulator-min-microvolt = <1800000>;
            regulator-max-microvolt = <3300000>;
            regulator-boot-on;
            regulator-always-on;
        };

        ldo4_reg: regulator@6 {
            /* +3.3V voltage with ±4% tolerance */
            regulator-min-microvolt = <1800000>;
            regulator-max-microvolt = <3300000>;
            regulator-boot-on;
            regulator-always-on;
        };
    };
};

i2cdump -f -y 1 0x1b
No size specified (using byte-data access)
     0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f    0123456789abcdef
00: 00 00 00 10 04 00 00 00 00 00 00 01 00 00 00 80    ...??......?...?
10: 80 ff ff 78 78 78 78 78 78 06 00 fe 00 00 fe 00    ?..xxxxxx?.?..?.
20: 00 00 00 00 00 00 00 00 00 00 00 80 80 00 00 00    ...........??...
30: 00 00 00 04 00 00 00 00 00 00 04 00 00 00 00 00    ...?......?.....
40: 00 04 00 00 00 00 00 00 04 00 00 00 00 00 00 00    .?......?.......
50: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
60: 00 00 00 00 00 c0 02 00 00 00 00 00 00 00 00 00    .....??.........
70: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
80: 00 00 00 10 04 00 00 00 00 00 00 01 00 00 00 80    ...??......?...?
90: 80 ff ff 78 78 78 78 78 78 06 00 fe 00 00 fe 00    ?..xxxxxx?.?..?.
a0: 00 00 00 00 00 00 00 00 00 00 00 80 80 00 00 00    ...........??...
b0: 00 00 00 04 00 00 00 00 00 00 04 00 00 00 00 00    ...?......?.....
c0: 00 04 00 00 00 00 00 00 04 00 00 00 00 00 00 00    .?......?.......
d0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
e0: 00 00 00 00 00 c0 02 00 00 00 00 00 00 00 00 00    .....??.........
f0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................

尝试强制把下面的寄存器powerup起来 似乎也不奏效

/* Line1 Input control registers */
#define LINE1L_2_LADC_CTRL        19
#define LINE1R_2_LADC_CTRL        21
#define LINE1R_2_RADC_CTRL        22
#define LINE1L_2_RADC_CTRL        24
/* Line2 Input control registers */
#define LINE2L_2_LADC_CTRL        20
#define LINE2R_2_RADC_CTRL        23