This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS 6.1的workspace问题



我用ccs6.1.

1、弄了好几个workspace,然后觉得太多了,看着不顺眼,想删掉几个,在哪里删?只能添加,无法删除?

2、在一个workspace下,打开某个工程,跳出Issue,在details里面提示是“A resource exists on disk with a different case E:\........”导致这个工程再也打不开,改个名字才能打开。但是我在其他workspace下都没发开过该工程。我不想改工程名字,这该怎么弄?

  • 试试:

    http://processors.wiki.ti.com/index.php/Troubleshooting_CCSv5#General_IDE

    3. Clean the workspace (or try using a new one): CCS stores various information in a folder called '.metadata' located in the user's workspace. The contents of this folder can get corrupted over time, causing various instability and strange behavior. Using a new workspace or cleaning the old workspace often helps resolve these issues. To use a new workpspace, simply select a new workspace location ('File->Switch Workspace'). If you wish to clean the old workspace, the simplest way to do this is to delete the '.metadata' folder in the workspace. This will essentially reset the workspace and restore the environment to the default behavior. All projects that were in the workspace will need to be re-imported into CCS, even though they are still physically in the workspace folder. Also note that any modified preference settings will be lost (set back to the default setting). If you wish to avoid resetting those preferences, export the preferences to a file (outside the workspace) by selecting 'File->Export...->General->Preferences->To preference file' before deleting the workspace. Once the workspace has been cleaned, those preferences can be imported back into CCS by selecting 'File->Import...->General->Preferences->From preference file'

  • 删除文件我试过的。

    旧的“ delete the '.metadata' folder”删掉后,在CCS的File->Switch Workspace下还是有旧的workspace的链接,就是这里不知道怎么彻底删。

    如果不小心点了这个旧的链接,在文件下又产生了.metadata了。

  • 菜单Window->preferences