This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

emmc设备无法识别

Other Parts Discussed in Thread: AM3354

linux操作系统,am3354的芯片。

我的系统用SD卡,启动,启动过程中发现了emmc设备,但是在设备名下面找不到mmcblk1的设备

mmc0是SD卡设备,mmc1是emmc设备,开机log发现了emmc设备

[ 1.712316] Waiting for root device /dev/mmcblk0p2...
[ 1.788103] mmc0: host does not support reading read-only switch. assuming write-enable.
[ 1.798963] mmc0: new high speed SDHC card at address aaaa
[ 1.805207] mmcblk0: mmc0:aaaa SS08G 7.40 GiB
[ 1.814434] mmcblk0: p1 p2
[ 1.833521] kjournald starting. Commit interval 5 seconds
[ 1.839329] EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode
[ 1.846562] VFS: Mounted root (ext3 filesystem) readonly on device 179:2.
[ 1.853974] Freeing init memory: 236K
INIT: version 2.88 booting
[ 2.028663] mmc1: new high speed MMC card at address 0001
[ 2.035532] mmcblk1: mmc1:0001 DS2008 7.28 GiB
[ 2.040624] mmcblk1boot0: mmc1:0001 DS2008 partition 1 4.00 MiB
[ 2.047285] mmcblk1boot1: mmc1:0001 DS2008 partition 2 4.00 MiB

但是在/dev/的目录下找不到相应的设备   mmcblk0是SD设备,没找到mmcblk1设备

root@am335x-evm:~# ls /dev
mmcblk0                   tty0                      tty41                    urandom
mmcblk0p1              tty1                      tty42                    usbdev1.1
mmcblk0p2              tty10                    tty43                    usbdev1.2
mtab                          tty11                    tty44                    vcs