This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

omapl138移植Linux进入到内核之后调试串口打印不出东西



uboot引导kernel之后可以通过在内核代码里面加gpio拉高拉低证明内核确实跑进去了,bootargs里面配置了ttyS2,因为内核对控制台进行重定向之前内核打印的初始化在uncompress.h里面的,有两个话:putstr("Uncompressing Linux...");putstr(" done, booting the kernel.\n");这两句话是重定向之前打印的,可以在串口中看到,还有网上有人说可能是机器码不对,我也用gpio印证了machine_is_davinci_da850_evm()这个宏是真的。

这个问题已经困扰我两天了,这是我移植的第二块omapl138的板子,之前一块用的是nand作为存储,LCD控制器作为显示,调试串口为ttyS0,这一块用的是SPI FLASH做存储,emifa作为显示接口,调试端口为ttyS2上个礼拜把最小系统移植到第二块板子上,而且串口打印全部都有,这周一只是修改了显示的底层接口,编译出来就没有任何打印了,只怪自己上周最小系统的内核版本没有备份,搞得现在这么被动。

今天把第一块nand板子的内核代码拿出来,把bootargs中串口改为ttyS2,而且把重定向之前的串口初始化也改为ttyS2,可以看到putstr("Uncompressing Linux...");putstr(" done, booting the kernel.\n");这两句打印。

有没有人能给我点指导性的意见,bootargs和bootcmd这些已经核对了很多次了,而且都是之前成功的参数,机器码也核对了是正确的,通过拉gpio也确实跑进了内核,毫无头绪了!!!