This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

实现AM335x与FPGA的数据通信,硬件设计由ARM的GPMC接口,采用异步传输数据的方式。现能收到ARM发送给FPGA的片选信号和写有效信号,但是没有数据输出



应用ti的ti-sdk-am335x-evm-07.00.00.00版SDK软件包。请问都需要进行哪些配置修改,才能实现GPMC接口与FPGA的数据通信。多谢

  • 你已经做了哪些修改呢?

    在dts中

    1、需要配置pinmux

    2、需要配置gpmc

  • 谢谢您的回复!

    pinmux配置如下:

    fpga_pins_default: fpga_pins_default {
                pinctrl-single,pins = <
                    0x0 (PIN_INPUT_PULLUP | MUX_MODE0)  /* gpmc_ad0.gpmc_ad0 */
                    0x4 (PIN_INPUT_PULLUP | MUX_MODE0)  /* gpmc_ad1.gpmc_ad1 */
                    0x8 (PIN_INPUT_PULLUP | MUX_MODE0)  /* gpmc_ad2.gpmc_ad2 */
                    0xc (PIN_INPUT_PULLUP | MUX_MODE0)  /* gpmc_ad3.gpmc_ad3 */
                    0x10 (PIN_INPUT_PULLUP | MUX_MODE0) /* gpmc_ad4.gpmc_ad4 */
                    0x14 (PIN_INPUT_PULLUP | MUX_MODE0) /* gpmc_ad5.gpmc_ad5 */
                    0x18 (PIN_INPUT_PULLUP | MUX_MODE0) /* gpmc_ad6.gpmc_ad6 */
                    0x1c (PIN_INPUT_PULLUP | MUX_MODE0) /* gpmc_ad7.gpmc_ad7 */
                    0x20 (PIN_INPUT_PULLUP | MUX_MODE0) /* gpmc_ad8.gpmc_ad0 */
                    0x24 (PIN_INPUT_PULLUP | MUX_MODE0) /* gpmc_ad9.gpmc_ad1 */
                    0x28 (PIN_INPUT_PULLUP | MUX_MODE0) /* gpmc_ad10.gpmc_ad2 */
                    0x2c (PIN_INPUT_PULLUP | MUX_MODE0) /* gpmc_ad11.gpmc_ad3 */
                    0x30 (PIN_INPUT_PULLUP | MUX_MODE0) /* gpmc_ad12.gpmc_ad4 */
                    0x34 (PIN_INPUT_PULLUP | MUX_MODE0) /* gpmc_ad13.gpmc_ad5 */
                    0x38 (PIN_INPUT_PULLUP | MUX_MODE0) /* gpmc_ad14.gpmc_ad6 */
                    0x3c (PIN_INPUT_PULLUP | MUX_MODE0) /* gpmc_ad15.gpmc_ad7 */
                    /*0x40 (PIN_OUTPUT | MUX_MODE1)
                    0x44 (PIN_OUTPUT | MUX_MODE1)
                    0x48 (PIN_OUTPUT | MUX_MODE1)
                    0x4c (PIN_OUTPUT | MUX_MODE1)
                    0x50 (PIN_OUTPUT | MUX_MODE1)
                    0x54 (PIN_OUTPUT | MUX_MODE1)
                    0x58 (PIN_OUTPUT | MUX_MODE1)
                    0x5c (PIN_OUTPUT | MUX_MODE1)
                    0x60 (PIN_OUTPUT | MUX_MODE1)
                    0x64 (PIN_OUTPUT | MUX_MODE1)
                    0x68 (PIN_OUTPUT | MUX_MODE1)
                    0x6c (PIN_OUTPUT | MUX_MODE1)*/
                    0x70 (PIN_INPUT_PULLUP | MUX_MODE0) /* gpmc_wait0.gpmc_wait0 */
                    0x74 (PIN_INPUT_PULLUP | MUX_MODE7) /* gpmc_wpn.gpio0_30 */
                    0x80 (PIN_OUTPUT | MUX_MODE0)       /* gpmc_csn1.gpmc_csn1  */
                    0x90 (PIN_OUTPUT | MUX_MODE0)       /* gpmc_advn_ale.gpmc_advn_ale */
                    0x94 (PIN_OUTPUT | MUX_MODE0)       /* gpmc_oen_ren.gpmc_oen_ren */
                    0x98 (PIN_OUTPUT | MUX_MODE0)       /* gpmc_wen.gpmc_wen */
                    0x9c (PIN_OUTPUT | MUX_MODE0)       /* gpmc_be0n_cle.gpmc_be0n_cle */
                >;
            };

            nandflash_pins_sleep: nandflash_pins_sleep {
                pinctrl-single,pins = <
                    0x0 (PIN_INPUT_PULLDOWN | MUX_MODE7)
                    0x4 (PIN_INPUT_PULLDOWN | MUX_MODE7)
                    0x8 (PIN_INPUT_PULLDOWN | MUX_MODE7)
                    0xc (PIN_INPUT_PULLDOWN | MUX_MODE7)
                    0x10 (PIN_INPUT_PULLDOWN | MUX_MODE7)
                    0x14 (PIN_INPUT_PULLDOWN | MUX_MODE7)
                    0x18 (PIN_INPUT_PULLDOWN | MUX_MODE7)
                    0x1c (PIN_INPUT_PULLDOWN | MUX_MODE7)
                    0x70 (PIN_INPUT_PULLDOWN | MUX_MODE7)
                    0x74 (PIN_INPUT_PULLDOWN | MUX_MODE7)
                    0x7c (PIN_INPUT_PULLDOWN | MUX_MODE7)
                    0x90 (PIN_INPUT_PULLDOWN | MUX_MODE7)
                    0x94 (PIN_INPUT_PULLDOWN | MUX_MODE7)
                    0x98 (PIN_INPUT_PULLDOWN | MUX_MODE7)
                    0x9c (PIN_INPUT_PULLDOWN | MUX_MODE7)
                >;
            };

    pinmux里没有配置nand了。

    gpmc配置如下:

    gpmc: gpmc@50000000 {
                status = "okay";
                pinctrl-names = "default";//, "sleep";
                pinctrl-0 = <&fpga_pins_default>;
                //pinctrl-1 = <&nandflash_pins_sleep>;
                ranges = <0 0 0x08000000 0x10000000>,
                     <1 0 0x20000000 0x08000000>;   /* CS0: NAND */
                nand@0,0 {
                    reg = <0 0 0>; /* CS0, offset 0 */
                    nand-bus-width = <16>;
                    gpmc,device-width = <1>;
                    gpmc,sync-clk-ps = <0>;
                    gpmc,cs-on-ns = <0>;
                    gpmc,cs-rd-off-ns = <44>;
                    gpmc,cs-wr-off-ns = <44>;
                    gpmc,adv-on-ns = <6>;
                    gpmc,adv-rd-off-ns = <34>;
                    gpmc,adv-wr-off-ns = <44>;
                    gpmc,we-on-ns = <0>;
                    gpmc,we-off-ns = <40>;
                    gpmc,oe-on-ns = <0>;
                    gpmc,oe-off-ns = <54>;
                    gpmc,access-ns = <64>;
                    gpmc,rd-cycle-ns = <82>;
                    gpmc,wr-cycle-ns = <82>;
                    gpmc,wait-on-read = "true";
                    gpmc,wait-on-write = "true";
                    gpmc,bus-turnaround-ns = <0>;
                    gpmc,cycle2cycle-delay-ns = <0>;
                    gpmc,clk-activation-ns = <0>;
                    gpmc,wait-monitoring-ns = <0>;
                    gpmc,wr-access-ns = <40>;
                    gpmc,wr-data-mux-bus-ns = <0>;
                    ti,nand-ecc-opt= "bch8";
                    ti,elm-id = <&elm>;
                    /* MTD partition table */
                            /* All SPL-* partitions are sized to minimal length
                     * which can be independently programmable. For
                     * NAND flash this is equal to size of erase-block */
                    #address-cells = <1>;
                    #size-cells = <1>;
                    partition@0 {
                        label = "NAND.SPL";
                        reg = <0x00000000 0x000020000>;
                    };
                    partition@1 {
                        label = "NAND.SPL.backup1";
                        reg = <0x00020000 0x00020000>;
                    };
                    partition@2 {
                        label = "NAND.SPL.backup2";
                        reg = <0x00040000 0x00020000>;
                    };
                    partition@3 {
                        label = "NAND.SPL.backup3";
                        reg = <0x00060000 0x00020000>;
                    };
                    partition@4 {
                        label = "NAND.u-boot-spl-os";
                        reg = <0x00080000 0x00040000>;
                    };
                    partition@5 {
                        label = "NAND.u-boot";
                        reg = <0x000C0000 0x00100000>;
                    };
                    partition@6 {
                        label = "NAND.u-boot-env";
                        reg = <0x001C0000 0x00020000>;
                    };
                    partition@7 {
                        label = "NAND.u-boot-env.backup1";
                        reg = <0x001E0000 0x00020000>;
                    };
                    partition@8 {
                        label = "NAND.kernel";
                        reg = <0x00200000 0x00800000>;
                    };
                    partition@9 {
                        label = "NAND.file-system";
                        reg = <0x00A00000 0x0F600000>;
                    };
                };
               
                nor@1,0 {
                    compatible = "cfi-flash";
                    #address-cells = <1>;
                    #size-cells = <1>;
                    reg = <1 0 0x08000000>;
                    bank-width = <2>;

                    /*gpmc,mux-add-data = <2>;
                    gpmc,cs-on-ns = <0>;
                    gpmc,cs-rd-off-ns = <186>;
                    gpmc,cs-wr-off-ns = <186>;
                    gpmc,adv-on-ns = <12>;
                    gpmc,adv-rd-off-ns = <48>;
                    gpmc,adv-wr-off-ns = <48>;
                    gpmc,oe-on-ns = <54>;
                    gpmc,oe-off-ns = <168>;
                    gpmc,we-on-ns = <54>;
                    gpmc,we-off-ns = <168>;
                    gpmc,rd-cycle-ns = <186>;
                    gpmc,wr-cycle-ns = <186>;
                    gpmc,access-ns = <114>;
                    gpmc,page-burst-access-ns = <6>;
                    gpmc,bus-turnaround-ns = <12>;
                    gpmc,cycle2cycle-delay-ns = <18>;
                    gpmc,wr-data-mux-bus-ns = <90>;
                    gpmc,wr-access-ns = <186>;
                    gpmc,cycle2cycle-samecsen;
                    gpmc,cycle2cycle-diffcsen;*/

                    /*partition@0 {
                        label = "bootloader-nor";
                        reg = <0 0x40000>;
                    };
                    partition@0x40000 {
                        label = "params-nor";
                        reg = <0x40000 0x40000>;
                    };
                    partition@0x80000 {
                        label = "kernel-nor";
                        reg = <0x80000 0x200000>;
                    };
                    partition@0x280000 {
                        label = "filesystem-nor";
                        reg = <0x240000 0x7d80000>;
                    };*/
                };
            };
        };

    硬件fpga的片选为CS1。请您帮忙看看是否有不对的地方,多谢

  • 没有人知道么?请求帮助啊!多谢