This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

用DSP/BIOS能实现TCP/UDP数据传输吗?



各位大神好!

在CCSv5.2中使用DSP/BIOS,版本为bios_5_41_13_42, 现需要实现网络数据传输,即基于TCP和UDP进行网络数据传输。我知道基于SYS/BIOS可以利用ndk实现tcp传输。迫于项目需要,必须使用DSP/BIOS实现这一功能。

请问用DSP/BIOS能实现TCP/UDP数据传输吗?如果可以的话,应该怎样具体实现呢?

希望各路大侠帮帮小妹,不胜感激!