我现在想通过8168的sata口连接2.5英寸笔记本硬盘,实现对压缩后的视频进行存储。请问我新买的硬盘,需要对移动硬盘进行什么处理吗?我已经在win7下格式化为ntfs格式,但还是不能正确建立连接,我已经给硬盘外接5V供电了。谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我现在想通过8168的sata口连接2.5英寸笔记本硬盘,实现对压缩后的视频进行存储。请问我新买的硬盘,需要对移动硬盘进行什么处理吗?我已经在win7下格式化为ntfs格式,但还是不能正确建立连接,我已经给硬盘外接5V供电了。谢谢
Mike,
默认的Linux是不支持NTFS的。
建议在Linux下格式化为ext3.
谢谢你的回复!我已经在Linux下格式化为ext3.但是如何实现开机自动挂载硬盘?我开机自动挂载不上!另外,我采用mount命令挂载成功,向硬盘写入的文件,能够在文件系统的挂载点上看到写入的文件吗?如何操作?谢谢