omapl38用网线连接交换机,可以使用socket实现和PC通信吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LINUX默认应该是支持网络的
如果你用TI提供的软件,没有任何修改的话,系统起来
先用udhcp -i eth0, 让网口获取IP
然后可以尝试PING网关
denny你好,我是直连的形式,但是ping的时候虽然能通,但是丢包率达到50%,omapl138的核心板。这是怎么个情况?
丢包率过高,可以检查一下硬件,主要看PHY周围电路,晶振,信号等质量是否合格。