自己做的板子,芯片am3352,电源tps65910a3,裸板串口0看不到打印信息 cccc都没有
现在基本所有串口接串口转usb,转接头串口有高电平3v3,这时板子不上电,测5v都会有0.9v这样的电压。是am3352被击穿了?电压怎么会到5v去。 假设am335x芯片由于高压击穿会是什么现象。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
击穿了可能到5v也可能到0,您测的电压是在AM335x侧测的,还是在232的片子后测的。
如果不能出CCC,你看看65910的输出是否正常,另外看看晶振是否起振。
也就是说,不开电情况下io不能接受超过0.3v电压。我uart0接了串口转usb,串口线在内部有上拉,导致uart0关机情况下也有电压,这样是否损坏了am3352芯片。串口转换器插在UART0上,我在不开机情况下测5v都有0.9v电压,这是为什么;有一块板子直接是1.8v,5v指示灯都亮了。芯片坏了?但是后面的怎么解释。
tps65910电压都是正确的。 各电压之间也没有短路请况。
晶振是起振的,而且XDMA_EVENT_INTR0 引脚,同说明书上一样If sysboot[5] is high on the rising edge or PWRONRSTn,
this terminal will initially be driven low after reset is released then it begins to toggle at the same frequency of the XTALIN terminal,也就是XDMA_EVENT_INTR0 引脚示波器量的24M起振信号。
而且测得,启电复位后的io高电平状态测了几个都是对的,UART0 tx rx 高电平,jtag 的TMS TDI高电平 这些是对于vddshv6的io。