This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
CCS5.1在linux连接仿真器是否需要专门的驱动,这个驱动在哪里有
你好,
ccs v5安装时自动安装驱动,不需要特别安装。
嗯,不是的CCS5,1自带的基本都是TI自己的仿真器,比如我使用SEED的XDS560PLUS那就没这个驱动了,所以感觉在Linux下面行不通了
还有个问题是连win下面,我的CCS5.1也使用不了这个仿真器。悲剧
不可能CCS不能使用SEED的XDS560PLUS仿真器,买仿真器的时候有没有送给你一个驱动光盘?针对它,安装它的驱动就行了。
嗯,你好,CCS5.1的话SEED还没有给出专门的驱动,有的只是CCS4的驱动。我现在的CCS是5.1的版本,其他版本当然可以使用。
这样的话,确实需要等SEED发布该仿真器CCS V5.1的驱动了,祝你好运。