8148的电源参考EVM8148采用tps6591133,没给芯片通电之前调试电源电压都正常。通上电之后发现tps6591133发热,之后发现把PLL_1V8和CORE_VDD两路电源断开后,电源芯片不再发热,电压也正常。测量板子发现8148的PLL_1V8对地短路,CORE_VDD正常。CORE_VDD为1.2V,PLL_1V8是1.79V.现在苦于找不到短路原因,求大神帮忙,万分感谢!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
8148的电源参考EVM8148采用tps6591133,没给芯片通电之前调试电源电压都正常。通上电之后发现tps6591133发热,之后发现把PLL_1V8和CORE_VDD两路电源断开后,电源芯片不再发热,电压也正常。测量板子发现8148的PLL_1V8对地短路,CORE_VDD正常。CORE_VDD为1.2V,PLL_1V8是1.79V.现在苦于找不到短路原因,求大神帮忙,万分感谢!!!
Chi Xiaoyan,
如果是新板子,建议先把电源焊上,测量电压输出正常后再焊上主芯片。
检查一下原理图和pcb,看看是有什么错误。
电源到芯片电源引脚都是0ou电阻隔开的,但是有的电源比如ddr电源我没有供电,因为只想用最小系统工作,难道是因为有的电源没供上电导致这一路烧了?