如题,请问,AM335X 支持ddr3 400吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
400MHz的无vtt设计最好参考BBB板子的layout,这个是经过了验证的。
http://circuitco.com/support/index.php?title=BeagleBoneBlack
我的板子设置 DDR 366有的可以跑,有点跑的不稳定,设置DDR 333基本稳定。 有可能是配置问题吗?
具体不稳定的情况,是DDR读写错误么?有做过DDR的仿真么?
terry xie 说:我的板子设置 DDR 366有的可以跑,有点跑的不稳定,设置DDR 333基本稳定。 有可能是配置问题吗?
不建议跑这个频率,跑400,或者333,或者303