我手上有块公司的 AM335的GP验证板,现在启动的时候,出现了下面的问题,烦请指教指教!!!!
Starting Dropbear SSH server: dropbear.
Starting telnet daemon.
Starting syslogd/klogd: done
Starting thttpd.
Starting PVR
find: /lib/modules/3.14.43-g875c69b: No such file or directory
Error: missing filename.
Could not find pvrsrvkm driver
Starting Lighttpd Web Server: 2014-03-25 09:04:01: (log.c.166) server started
lighttpd.
/
Starting Matrix GUI application.
***************************************************************
***************************************************************
NOTICE: This file system contains the followin GPLv3 packages:
binutils-symlinks
binutils
gdbserver
If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
Stopping Bootlog daemon: bootlogd.
INIT: Id "S" respawning too fast: disabled for 5 minutes
INIT: Id "S" respawning too fast: disabled for 5 minutes
另外,请问TI官方有am335的如何制作文件系统的文档么,在TI的官网上没找到,也不晓得TI的文件系统中的文件是不是有什么特殊的要求!!!