主板DM8148加外围硬件底板,主板在另一块2#硬件底板验证是ok,验证1#硬件底板时,外围设备几乎都不能用,几乎都是报错 omap_i2c omap_i2c.1: controller timed out,请问是底板硬件的问题?还是软件有bug?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Xiao Dong,
主板加2#底板的I2C操作是否正常? 如果是,先测量一下1#底板I2C信号。两块板子连接是否紧密。
Xiao Dong,
请测量软件有操作I2C是时候主板上I2C时钟和数据信号,已经远端底板上I2C时钟和数据信号。#1和#2底板的原理图和pcb是完全一样的,对么?
Dong Xiao 说:1#底板出现I2C0_SCL电平较2#底板信号一半还低,
问题还是信号不正常导致的。由于主板和2#底板工作正常,所以主板输出的I2C信号应该是正确的。你能否测量一下底板和主板接口处的I2C信号是否就不正常了?
Dong Xiao 说:一个奇怪的现象发生,用紅表笔接scl黑表笔接sda出现短路,而红表笔接scl黑表笔接sda则不会出现短路报警
测量电容就是这样的现象。
你看看pcb上有没有什么多余的焊锡。
Dong Xiao 说:3:1#底板单独上电,SCL电平664mv(2#底板忽略不计) SDA电平381mv(2#底板忽略不计)
查查电压从哪里来的? 是不是之前的短路导致底板上什么芯片坏了?