问下大家,我的内核是2.6.12的,我的遇到的问题是lsusb,回车,屏幕什么都没输出,在我连接4G模块后,也打印出了什么ttyUSB0 1 2了,但是实际dev下并没有,我收到创建节点后,打开ttyUSB0和1正常,0可以发数据,如果我发ATZ\r\n,返回好多AAAAAAAAAAAA。。。ATZ\r\n ERROR ,打开ttyUSB2直接崩溃,我命令用的cat ttyUSBx & echo "ATZ\r\n" >>/dev/ttyUSBx 。出错的打印在附件中
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
问下大家,我的内核是2.6.12的,我的遇到的问题是lsusb,回车,屏幕什么都没输出,在我连接4G模块后,也打印出了什么ttyUSB0 1 2了,但是实际dev下并没有,我收到创建节点后,打开ttyUSB0和1正常,0可以发数据,如果我发ATZ\r\n,返回好多AAAAAAAAAAAA。。。ATZ\r\n ERROR ,打开ttyUSB2直接崩溃,我命令用的cat ttyUSBx & echo "ATZ\r\n" >>/dev/ttyUSBx 。出错的打印在附件中
我们用的DM368的,dma已经关掉了,优盘都是工作正常的,是不是驱动要改一些。
Li Qiankun,
请问4G模块的供应商是否有提供给你们Linux PC下驱动的源码,供你们参考?
U盘使用的是mass storage的USB驱动,和4G模块不一样的。
没有提供,但是我在368上同样打开pl2303的驱动,插入后也能正确识别,短接rxtx,收了一大堆乱码,是不是和usbseial的驱动有问题,更底层的应该没问题,串口和U盘都是块传输 。