This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAN8720的晶振波形幅值变化大



用am335x+LAN8720做了一个百兆网口,LAN8720使用的外部50M晶振,调试中发现,晶振输出波形周期正常,但是幅值会在3.1V到4.16V之间来回跳变,这导致网口的丢包率特别严重,能达到25%到35%。各位,有没有遇到类似的问题?

50M晶振和LAN8720、CPU之间分别串联了一个22Ω的电阻,之前的板子上,晶振和LAN8720之间是直连的,没有串阻,也没发现丢包的问题,但是现在把串阻去掉,晶振波形还是不对,真是不知道哪里的问题了。