This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TVP5154/TVP5158

Other Parts Discussed in Thread: TVP5154

最近在使用TVP5154作为视频解码芯片,其datasheet里提到过图像增强相关内容,想请问一下它的图像增强体现在哪些方面并如何实现的?

  • Jerry,

    TVP5154的手册上有如下描述,应该是芯片硬件设计本身就提高图像的高频信号信息,例如锐度。

    4.5 Luminance Processing
    The luma component is derived from the composite signal by subtracting the remodulated chroma
    information. A line delay exists in this path to compensate for the line delay in the adaptive comb filter in
    the color processing chain. The luma information is then fed into the peaking circuit, which enhances the
    high-frequency components of the signal, thus, improving sharpness.

    其他请参考资源帖:http://www.deyisupport.com/question_answer/dsp_arm/davinci_digital_media_processors/f/39/t/52747.aspx。

  • 图像增强这块,包括对比度饱和度增益等等图像后处理方面,也包括前面提到的对于视频信号CVBS本身采集的增强方面,比如对于弱信号的增强,非标信号的兼容等