This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
.out文件转换成.bin文件可以参考bootloader文档上的例子。2.3.3.1 Using the HEX55 Utility to Create an Output Filehttp://www.ti.com/lit/an/spra763c/spra763c.pdf
可以看一下EHPI boot的原理2.3.3 EHPI Boot Mode
0x10000处放的是你程序要执行的第一条指令.
-cr选项在ccs->Show Build Settings->C5500 Linker->Runtime Enviroment->Iniitialization model
你要把_c_int00地址设为0x10000. 请参考下面的wiki网站。http://processors.wiki.ti.com/index.php/Accessing_c_int00
谢谢分享!