This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6657通过hyperlink boot不稳定,请教?



我的板上有2个C6657,DSP1通过SPI boot,DSP2通过hyperlink由DSP1实现boot

1. 上电后,先复位DSP2, 然后复位DSP1

2. DSP1能正常boot运行

3. 但DSP2有时能够boot运行起来,大多时候boot不起来,不稳定。

    在DSP2没能boot运行时,这时候如果我在CCS中启用仿真器连接DSP一下,DSP2就boot运行起来了。

 

请问,这可能是什么原因?