This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

5502的外扩flash

现在用的5502与SST39VF040连接,采用异步16bit的数据格式,flash为8位,连接CE2,首地址0x800000
现在要字寻址的话,首地址应该是0x400000吗?然后进行移位操作是左移1位还是2位?
比如写AA到flash的0x5555,地址是0x400000+0xAA*2(or 4)吗?

谢谢各位。