This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

5502的外扩flash



现在用的5502与SST39VF040连接,采用异步16bit的数据格式,flash为8位,连接CE2,首地址0x800000
现在要字寻址的话,首地址应该是0x400000吗?然后进行移位操作是左移1位还是2位?
比如写AA到flash的0x5555,地址是0x400000+0xAA*2(or 4)吗?

谢谢各位。

  • 你好,

    我觉得,首地址还是CE2的空间首地址0x800000。

    地址线看你是怎么连接的,如果是Internal Address A [20:1],应该是地址左移一位。

    过如果你有平台的话,可以试验一下,检验一下EMIF接口的信号。