四个deinterlace的D1想用一个dm368来编码
现在的问题是:
1. dm368是否支持创建4个编码通道?
2. 接口上如何输入,是4倍速度的bt656输入,还是在bt1120上输入?
3 输入的d1是interlace的,dm368能否支持deinterlace的滤波?
谢谢了
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Junbo Chu 说:1. dm368是否支持创建4个编码通道?
2. 接口上如何输入,是4倍速度的bt656输入,还是在bt1120上输入?
请参考Udworks的DM368 DVR的spec和设计。
Junbo Chu 说:3 输入的d1是interlace的,dm368能否支持deinterlace的滤波?
DM36x可以支持隔行编码,由解码端去做去交织。
Chu Junbo,
如果输入的高清信号是YUV422的,输入的标清信号是模拟CVBS信号,可以使用一个VIP口接1080p的数据,另外一个VIP+TVP5158接入4路模拟信号。