This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

davinci 芯片选型问题咨询



目前我准备开发一款摄像头模组,采用1300万像素的CMOS传感器,但是在选择ISP芯片的时候有点不确定。想咨询一下davinci系列是否有合适的芯片可以用作ISP。要求具有良好的3A功能,可以手动控制白平衡、自动曝光、自定义白平衡,手动设置曝光区域、白平衡区域、曝光补偿等参数

  • 应当是没有1300w的isp处理能力的处理器,dm8127也到不了1300w。

  • 你好,

    请问你13MP的帧率是多少?sensor的pclk是多少?如果pclk小于165Mhz,TI是有芯片可以支持的。

    3A包括自动白平衡,自动曝光,自动对焦。TI在自动对焦上没有相关算法软件。TI的IPNC软件里面有自动白平衡和自动曝光的软件,自动白平衡是提供库。自动曝光提供的是源码,可以可以修改。

  • 什么帧率? 在PCLK小于165MHz的情况下你仍然可以使用并口接入sensor。 超过的情况下,如果你的sensor支持MIPI那完全可以直接接入。MIPI的分辨率上限是非常高的。据我所知这颗芯片接24Mp都没有问题。