由于我们公司现在需要开发一个基于视频处理的系统,要使用TI公司的TMS320C6678的8核DSP芯片,
我如何创建一个MCSDK的工程,可以实现底层的芯片初始化和外设的驱动初始化,以实现8核DSP芯片的可启动,然后运行起来?
也就是说如何在CCS5.2中创建一个最小可启动的镜像系统?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
由于我们公司现在需要开发一个基于视频处理的系统,要使用TI公司的TMS320C6678的8核DSP芯片,
我如何创建一个MCSDK的工程,可以实现底层的芯片初始化和外设的驱动初始化,以实现8核DSP芯片的可启动,然后运行起来?
也就是说如何在CCS5.2中创建一个最小可启动的镜像系统?
我现在需要的不仅仅是裸跑的程序,而是创建一个MCSDK工程,其中包含有bios实时操作系统,还需要包含底层的芯片初始化和外设的驱动初始化,以实现TMS320C6678的8核DSP芯片的可启动,然后运行起来。
请问CCS5.2集成开发平台上是否有相似的例程?
如果有的话,是哪一个?
如果没有的话,该如何构建?