This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am335x支持网络和usb唤醒么



am335x支持网络和usb唤醒么

  • 我知道usb唤醒时可行的, 网络能行么

  • jd.f,

    http://processors.wiki.ti.com/index.php/AM335x_Power_Management_Standby_User's_Guide

    Ethernet wakeup for standby is not validated, as on EVM ETH PHY_WAKEUP pin is not hooked up to any GPIO pin.

  • 网络不行,但是USB印象中在DS1模式下应该是可以。

    8.1.4.5 Wakeup Sources/Events
    Following events will wake up the device from Deep sleep(low power) modes. These are part of the
    Wakeup Power domain and remain always ON.
    Note: For differences in operation based on AM335x silicon revision, see Silicon Revision Functional
    Differences and Enhancements, Silicon Revision Functional Differences and Enhancements.
    • GPIO0 bank
    • dmtimer1_1ms (timer based wakeup)
    • USB2PHY (USB resume signaling from suspend) – Both USB ports supported.
    • TSC (touch screen controller, ADC monitor functions )
    • UART0 (Infra-red support)
    • I2C0
    • RTC alarm

    特别提一下,AM335x支持多种低功耗的模式,所以建议你一定要仔细核对TRM的8.1.4.3 Power Modes,确认自己选择的那种低功耗模式可以支持。