大家好,我使用的是TVP5151IPBSR这款芯片,希望只需要读取灰度图像进入MCU处理,但是这款芯片YOUT有8个引脚,请问:
1.我应该怎样读取才可以只读取到Y信号而不读取到UV信号呢?
2.当我设置好Color Killer 它是否只会输出Y信号呢?
3.为了使同步信号分离是否是应该在0Dh的Outputs and Data Rates Select Register这个寄存器的YCbCr output format位进行设置即可呢?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好,我使用的是TVP5151IPBSR这款芯片,希望只需要读取灰度图像进入MCU处理,但是这款芯片YOUT有8个引脚,请问:
1.我应该怎样读取才可以只读取到Y信号而不读取到UV信号呢?
2.当我设置好Color Killer 它是否只会输出Y信号呢?
3.为了使同步信号分离是否是应该在0Dh的Outputs and Data Rates Select Register这个寄存器的YCbCr output format位进行设置即可呢?
谢谢!
李泽贤 说:1.我应该怎样读取才可以只读取到Y信号而不读取到UV信号呢?
我看了一下TVP5151的手册,输出只能是YUV422的,即使图像的色度信息是没有的,还是会先输出8bit Y,然后8bit UV的。
李泽贤 说:这个时间节点有什么办法来同步保证吗?
你可以看看数据手册的Figure 3-6. Horizontal Synchronization Signals,一行Y,一行UV。
你也可以到网上搜索一下BT601的时序。