现在用am3352 + sdk6.0 + Qt5.5开发程序,但编译出来的程序在板子上跑窗口没有标题栏,弹窗不能拖动。
网上搜了需要窗体管理器,需要安装x window请问怎么弄。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
目前我接触到的客户中还没有人做过,不过你可以参考E2E上的这个指导进行尝试:
http://e2e.ti.com/support/arm/sitara_arm/f/791/t/419732
There isn't a recipe that you can bitbake to build your gnome x-window support in the fs.
You should either create your custom gnome recipe, which you can bitbake, or you can add the downloaded packages to the current core-sdk recipe.
You can refer to the following community wikis for directions on how to add the packages to your recipe:
www.yoctoproject.org/.../dev-manual.html
www.yoctoproject.org/.../dev-manual.html
stackoverflow.com/.../how-to-write-own-package-for-recipe-in-arago-project-build
arago-project.org/.../Main_Page
感觉还是qt的配置问题,会不会是板子上的qt特效没有打开。
请问qt特效指的是什么?怎么打开?我查看了QT的 ./configure --help,没看到相关的选项,有没有可能是3352没有GPU造成的?
这是我的配置
./configure \
-prefix /usr/local/qt-5.5.1-arm \
-device linux-am3352-g++ \
-device-option CROSS_COMPILE=~/ti-sdk-am335x-evm-06.00.00.00/linux-devkit/sysroots/i686-arago-linux/usr/bin/arm-linux-gnueabihf- \
-release \
-confirm-license \
-opensource \
-no-opengl \
-no-eglfs \
-nomake examples \
-v
GPU造成有可能了。
应用层的东西,您就多google下了,我们这边对应用层没有支持。
谢谢!