This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6657 EMIF16 接口测试



你好!我在调试C6657的EMIF16接口连接FPGA时遇到一些疑惑和问题!希望能得到TI的解答:

1>在查看《External Memory Interface (EMIF16)》(SPRUGZ3A May 2011)手册中发现C6657是支持ASRAM的,所以打算将FPGA设计成RAM供C6657读写,但是所有配置寄存器并没有找到和ASRAM相关的配置,调试STK_EMIF历程时,发现ASRAM的配置和Norflash是一致的,而且查看配置寄存器在接口模式选择中只有A).Nanflash和B).禁止Nandflash两种(NANDFCR),-----------------这是不是说SRAM的地址和数据线和Norflash是一样的所以在接口上可以通用

2> 如图是修改的STK历程,在所用硬件上是可以通过STK_EMIF的Nanflash测试示波器也能测到OE的跳变,改成Norflash模式后通过往0x70000000地址写数据但是在memory中并没有看到数据的跟新,同时示波器也检测不到OE的跳变!-------这样访问EMIF16的CE0有问题吗?如果有问题那该如何访问进行CE0的读写?期待您的回答谢谢