板子本身是没有问题的。使用linux3.2的内核已经移植成功了。
但是移植到内核4.1之后, 文件系统开始挂载之后, 调试串口出现假死情况。
最后时刻的log
run-parts: /etc/network/if-up.d: No such file or directory
done.
hwclock: can't open '/dev/misc/rtc': No such file or directory
Thu Jan 1 01:21:00 UTC 1970
hwclock: can't open '/dev/misc/rtc': No such file or directory
INIT: Entering runlevel: 5
Starting system message bus: [ 8.116494] random: dbus-daemon urandom read with 46 bits of entropy available
Failed to start message bus: Failed to read directory "/etc/dbus-1/system.d": No such file or directory
Starting telnet daemon.
hwclock: can't open '/dev/misc/rtc': No such file or directory
Starting syslogd/klogd: done
Stopping Bootlog daemon: bootlogd.
在这条log之后没有再向调试串口输入信息不会有任何反应。