提示“unable to load C:\CCStudio_v3.3\drivers\tixds560icepick_c.dvr”,查过相应的文件夹目录,这个文件是存在的。
CCS的具体版本号是:CCS3.3.83.19。
ccs setup里面是import的logic pd的C6748_tixds560.ccs。请问这是怎么回事?多谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
解决了,比较奇怪CCS3.3.83.19还是在logic pd的L138的相关下载里下载的,我换成低版本的CCS3.3.82.13就可以连接上了。按说高版本应该兼容低版本的特性,不知道是怎么回事!另外咨询一下JTAG仿真器连接spectrum的L137板子时,boot的拨码开关无论拨到哪种模式下,仿真器都可以连接上; 而连接logic pd的L138板子时,必须将boot的拨码开关置到EMU Debug模式才能连接上,这个是芯片设计导致的不同?还是板子电路上有不同,L137的板子做了特殊设计?
你好,针对于CCS3.3,其实最高版本是CCS3.3.82.13这个版本,CCS3.3.83这个版本主要就是针对MCU的支持。很多C6000等一些芯片的选择都没有。如果你要是用MCU的话,建议可以升级到83这个版本。但是仿真C6000或者其他芯片,请升级到CCS3.3.82.13就可以了。
L137和L138的芯片设计是不一样的。L137的CCS连接过程是先连接DSP端,再连ARM端,然后再使用DSP端。而L138的CCS连接过程是先连接ARM端,再连接DSP端。注意所有连接之前一定要先加载好GEL文件。
还有连接之前,如果不设置boot模式,可以直接通过串口将系统停掉,或者连接之前按一下复位键。