自己做的板子。板上有4片DSP C6678,总共有2G DDR。目前测试的主要目的是,在1333MHz的速率下,DDR是否可以初始化正常,DDR是否会存在错误值。
当前的测试结果是:在1333MHz的速率下,前3片DSP的DDR初始化lever可以通过,第4片DSP的DDR初始化lever不通过,当降低速率到800MHz的时候,4片DSP的DDR初始化lever通过。但同时4片DDR的错误率都提高了。
这种情况是什么引起的?应该如何考虑并解决?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
自己做的板子。板上有4片DSP C6678,总共有2G DDR。目前测试的主要目的是,在1333MHz的速率下,DDR是否可以初始化正常,DDR是否会存在错误值。
当前的测试结果是:在1333MHz的速率下,前3片DSP的DDR初始化lever可以通过,第4片DSP的DDR初始化lever不通过,当降低速率到800MHz的时候,4片DSP的DDR初始化lever通过。但同时4片DDR的错误率都提高了。
这种情况是什么引起的?应该如何考虑并解决?
DDR的测试错误方法是:每个核一直做FFT,检查核0做FFT的结果,与存储在LL2中的FFT结果(正确结果)。若不一致,认为是错误。