This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

【Keystone Bootloader】6678用以太网启动方式的时候,如果有一个板子上有两个DSP都连到交换机上,怎么区分mac地址。

专家好:
1用以太网加载的时候,启动参数表的14 、16 、18总共6个字节存放了MAC地址,该地址是从哪里来的啊?是通过管教上下拉实现的吗?
2如果我板卡上有两个DSP,都连接到交换芯片上,PC分别给两个DSP加载程序的时候,怎么区分这两个DSP的?

  • 您好,

    在EMAC中的寄存器中存在默认的MAC地址,RBL起来后会去读取寄存器的值获取MAC值;

    每个DSP有独立的MAC地址,通过抓取DSP发送来的bootp包可以获得每个DSP的MAC地址,然后通过发包工具,向对应DSP发包即可。