This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM385 VIP 采集数据分立同步错误



DM385的VIP0采集分离同步数据的问题,前端芯片是GV7601/GS2971,时序是16bit YCbCr HVF 或者 HBLK(ACTVID)VBLK都测试过 
我们现在用VIP0的16bit数据线,HS,VS,DE,FD接了GV7601/GS2971的SDI Rx芯片,使用分立同步模式,做了如下实验,GV7601输出YCbCr 16bit 数据,用示波器看 PCLK = 74.25MHZ,VS=60Hz,HS=45kHz(720P60的画布是750行,750x60=45k行)
     a. SDI Rx芯片这边有2种时序,一种是HS-VS,一种是HBLK-VBLK(对应的是CPU这边的ACTVID_VBLK时序,需要把行有效区信号极性反一下);
     b. 通过VIP寄存器看,VIP0的配置是16bit,分立同步,那么结果是很诡异的,我们用压缩的视频流,以及VIP0直接采集420或者422的原始YUV数据做测试,结果是一致的,感觉是垂直是对的,水平方向采集到的图像是全的,就是
        整个Windows桌面的左侧和右侧是有的,中间感觉像是被均匀抽取了70%左右的数据;
        i.  HS+VS CPU采集到的数据是灰色的(灰场)
        i.  HS+VBLK CPU采集到的数据是1/4宽度的,如下图:
        i.  ACTVID+VBLK CPU采集不到数据;
        i.  如果直接用VIP里面的SC转420模式,会出现VIP Overflow;