This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSEVM6678L运行out-of-box的时候link找不到,该怎么办?



hyperterminal设置都是一样的:Bites per second:11500

Data bits:8bit

Parity:None

Stop bits:1

Flow control:None

编码格式我选择的UTF-8,然后是如下信息,进行不下去了,请问问题出在哪里?

POST result: PASS
IBL version: 1.0.0.16
IBL: PLL and DDR Initialization Complete
IBL Result code 00
IBL: Booting from NOR
platform_init Done
Start BIOS 6
QMSS successfully initialized
CPPI successfully initialized
PA successfully initialized
HUA version 2.00.00.04
Setting hostname to tidemo-102735
MAC Address: 00-17-EA-D1-43-43
Configuring DHCP client
PASS successfully initialized
Ethernet subsystem successfully initialized
Ethernet eventId : 48 and vectId (Interrupt) : 7
Registration of the EMAC Successful, waiting for link up ..
Service Status: DHCPC : Enabled : : 000
Service Status: THTTP : Enabled : : 000
Service Status: DHCPC : Enabled : Running : 000
Service Status: DHCPC : Enabled : Fault : 002
Service Status: DHCPC : Disabled : : 000
Service Status: DHCPC : Enabled : : 000
Service Status: DHCPC : Enabled : Running : 000
Service Status: DHCPC : Enabled : Fault : 002
Service Status: DHCPC : Disabled : : 000
Service Status: DHCPC : Enabled : : 000
Service Status: DHCPC : Enabled : Running : 000
Service Status: DHCPC : Enabled : Fault : 002
Service Status: DHCPC : Disabled : : 000
Service Status: DHCPC : Enabled : : 000
Service Status: DHCPC : Enabled : Running : 000

POST result: PASS
IBL version: 1.0.0.16
IBL: PLL and DDR Initialization Complete
IBL Result code 00
IBL: Booting from NOR
platform_init Done
Start BIOS 6
QMSS successfully initialized
CPPI successfully initialized
PA successfully initialized
HUA version 2.00.00.04
Setting hostname to tidemo-102735
MAC Address: 00-17-EA-D1-43-43
Configuring DHCP client
PASS successfully initialized
Ethernet subsystem successfully initialized
Ethernet eventId : 48 and vectId (Interrupt) : 7
Registration of the EMAC Successful, waiting for link up ..
Service Status: DHCPC : Enabled : : 000
Service Status: THTTP : Enabled : : 000
Service Status: DHCPC : Enabled : Running : 000
Service Status: DHCPC : Enabled : Fault : 002
Service Status: DHCPC : Disabled : : 000
Service Status: DHCPC : Enabled : : 000
Service Status: DHCPC : Enabled : Running : 000
Service Status: DHCPC : Enabled : Fault : 002
Service Status: DHCPC : Disabled : : 000
Service Status: DHCPC : Enabled : : 000
Service Status: DHCPC : Enabled : Running : 000
Service Status: DHCPC : Enabled : Fault : 002
Service Status: DHCPC : Disabled : : 000
Service Status: DHCPC : Enabled : : 000
Service Status: DHCPC : Enabled : Running : 000

  • 已经解决了,单机要装DHCP server 软件,而且最好用TI工程师提供的SERVER软件:http://www.deyisupport.com/question_answer/dsp_arm/c6000_multicore/f/53/p/18616/61914.aspx

    下载这里的软件,再运行就没问题了

  • 参考

    http://www.deyisupport.com/question_answer/dsp_arm/c6000_multicore/f/53/p/18616/61979.aspx#61979

    http://processors.wiki.ti.com/index.php/BIOS_MCSDK_2.0_User_Guide?keyMatch=EVM6678 out of box test&tisearch=Search-EN#Power_On_Self_Test_.28POST.29