问题描述:将beaglebone black板子使用SD卡将原生debian的系统换为了其官网的ubuntu,但在使用中偶尔会出现,给板子上电时,系统启动不起来,只有电源PWR灯是亮的,其他D2,D3,D4,D5灯都不亮,这时需要重新上电或者按一下power键板子才可能启动。问题遇到的概率5%左右。请问大家有没有遇到类似问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
问题描述:将beaglebone black板子使用SD卡将原生debian的系统换为了其官网的ubuntu,但在使用中偶尔会出现,给板子上电时,系统启动不起来,只有电源PWR灯是亮的,其他D2,D3,D4,D5灯都不亮,这时需要重新上电或者按一下power键板子才可能启动。问题遇到的概率5%左右。请问大家有没有遇到类似问题?
uboot命令行有输出错误信息么?直接加载kernel会报错么?
看现象,像是串口这部分有硬件串扰导致的,本来BBB的串口就是插针形式出来的。
U-boot的升级具体是指什么?更新U-boot的内容,要直接烧写存储介质。
因为从现象上看是在u-boot阶段误将串口的rx串扰信号识别为了anykey的按下动作,所以想通过修改u-boot代码部分中,只识别特定键按下才进入u-boot命令行的方法来规避串扰的anykey信号。但是发现beaglebone板子没有单独升级u-boot的命令,好像单独操作u-boot升级很麻烦。目前发现ubuntu16.04的版本已经将u-boot阶段autoboot倒计时处的anykey的识别变成了space键才进入u-boot命令行。但是还没测效果怎样。@ZhouJian谢谢您的解答。