This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM385 sd 卡映像写入不了SD 卡



我在DM385 上编译好了UBOOT 写入SD 卡,使用MKSD_TI81XX.SH 写入SD 卡,却总部成功是怎么回事?我的OS 版本是UBUNTU 16.04 ?

  • 你好;

            你是用的什么版本的SDK;

            是用的PNC_RDK_V3.8.0/Utils/sd-script/mksd-ti81xx.sh 这个文件吗?

            写入失败,有什么错误提示吗?

  • 如果是制作SD卡失败,你也可以手动了执行;

    用 fdisk 来重新分区;

    mkfs.vfat -F 32 -n boot "$1"1 &> /dev/null
    mkfs.ext3 -L rootfs "$1"2 &> /dev/null

    格式化2个分区,分别拷贝数据,具体看看 mksd-ti81xx.sh 的步骤就可以了

  • 我换了ubuntu12.04  出现

    sudo ./mksd-ti81xxuboot.sh /dev/sdb1 MLO u-boot.bin
    [sudo] password for hp:
    All data on /dev/sdb1 now will be destroyed! Continue? [y/n]
    y
    [Partitioning /dev/sdb1...]
    1024+0 records in
    1024+0 records out
    1048576 bytes (1.0 MB) copied, 0.00569995 s, 184 MB/s
    Disk /dev/sdb1 doesn't contain a valid partition table
    DISK SIZE - 1020788736 bytes
    CYLINDERS - 124
    Checking that no-one is using this disk right now ...
    BLKRRPART: Invalid argument
    OK
    Warning: start=2048 - this looks like a partition rather than
    the entire disk. Using fdisk on it is probably meaningless.
    [Use the --force option if you really want this]
    [Making filesystems...]
    [Copying files...]
    mount: special device /dev/sdb11 does not exist
    umount: /dev/sdb11: not found 

    这个怎么操作?

  • qigong du1 说:
    sudo ./mksd-ti81xxuboot.sh /dev/sdb1 MLO u-boot.bin

    你好;

            你的SD卡 是dev/sdb 吗? 你这里命令需要写 /dev/sdb ,   不是写/dev/sdb1

            这个脚本会重新对sd卡进行分区的,所以下面就报了,找不到sdb11了。

  • 我使用mount 命令查询了设备,显示的是   

    hp@hp:~/yourapp/Utils/sd-script$ mount
    /dev/sda1 on / type ext4 (rw,errors=remount-ro)
    proc on /proc type proc (rw,noexec,nosuid,nodev)
    sysfs on /sys type sysfs (rw,noexec,nosuid,nodev)
    none on /sys/fs/fuse/connections type fusectl (rw)
    none on /sys/kernel/debug type debugfs (rw)
    none on /sys/kernel/security type securityfs (rw)
    udev on /dev type devtmpfs (rw,mode=0755)
    devpts on /dev/pts type devpts (rw,noexec,nosuid,gid=5,mode=0620)
    tmpfs on /run type tmpfs (rw,noexec,nosuid,size=10%,mode=0755)
    none on /run/lock type tmpfs (rw,noexec,nosuid,nodev,size=5242880)
    none on /run/shm type tmpfs (rw,nosuid,nodev)
    gvfs-fuse-daemon on /home/hp/.gvfs type fuse.gvfs-fuse-daemon (rw,nosuid,nodev,user=hp)
    vmware-vmblock on /run/vmblock-fuse type fuse.vmware-vmblock (rw,nosuid,nodev,default_permissions,allow_other)
    /dev/sdb1 on /media/D602-2712 type vfat (rw,nosuid,nodev,uid=1000,gid=1000,shortname=mixed,dmask=0077,utf8=1,showexec,flush,uhelper=udisks)
    hp@hp:~/yourapp/Utils/sd-script$ 

    这个写/dev/sdb1应该是对的!

    现在我只想写UBOOT 和MLO ,一步一步的调试!

    #!/bin/bash

    if [[ -z $1 || -z $2 || -z $3 ]]
    then
    echo "mksd-ti814x Usage:"
    echo " mksd-ti814x <device> <MLO> <u-boot.bin> <uImage> <rootfs tar.gz >"
    echo " Example: mksd-ti814x /dev/sdc MLO u-boot.bin uImage nfs.tar.gz"
    exit
    fi

    if ! [[ -e $2 ]]
    then
    echo "Incorrect MLO location!"
    exit
    fi

    if ! [[ -e $3 ]]
    then
    echo "Incorrect u-boot.bin location!"
    exit
    fi

    #if ! [[ -e $4 ]]
    #then
    # echo "Incorrect uImage location!"
    # exit
    #fi

    #if ! [[ -e $5 ]]
    #then
    # echo "Incorrect rootfs location!"
    # exit
    #fi

    echo "All data on "$1" now will be destroyed! Continue? [y/n]"
    read ans
    if ! [ $ans == 'y' ]
    then
    exit
    fi

    echo "[Partitioning $1...]"

    DRIVE=$1
    dd if=/dev/zero of=$DRIVE bs=1024 count=1024

    SIZE=`fdisk -l $DRIVE | grep Disk | awk '{print $5}'`

    echo DISK SIZE - $SIZE bytes

    CYLINDERS=`echo $SIZE/255/63/512 | bc`

    echo CYLINDERS - $CYLINDERS
    {
    echo ,9,0x0C,*
    echo 10,,,-
    } | sfdisk -D -H 255 -S 63 -C $CYLINDERS $DRIVE

    echo "[Making filesystems...]"

    mkfs.vfat -F 32 -n boot "$1"1 &> /dev/null
    mkfs.ext3 -L rootfs "$1"2 &> /dev/null

    echo "[Copying files...]"

    mount "$1"1 /mnt
    cp $2 /mnt/MLO
    cp $3 /mnt/u-boot.bin
    #cp $4 /mnt/uImage
    umount "$1"1

    #mount "$1"2 /mnt
    #tar zxvf $5 -C /mnt &> /dev/null
    #chmod 755 /mnt
    #umount "$1"2

    echo "[Done]"

    我修改了SH 脚本,出现后 

    [Partitioning /dev/sdb1...]
    1024+0 records in
    1024+0 records out
    1048576 bytes (1.0 MB) copied, 0.00906893 s, 116 MB/s
    Disk /dev/sdb1 doesn't contain a valid partition table
    DISK SIZE - 1020788736 bytes
    CYLINDERS - 124
    Checking that no-one is using this disk right now ...
    BLKRRPART: Invalid argument
    OK
    Warning: start=2048 - this looks like a partition rather than
    the entire disk. Using fdisk on it is probably meaningless.
    [Use the --force option if you really want this]
    [Making filesystems...]
    [Copying files...]
    mount: special device /dev/sdb11 does not exist
    umount: /dev/sdb11: not found
    [Done]  

    实现只写MLO 和UBOOT 怎么操作?

  • 那你直接把mlo 和 uboot 直接拷贝到sd卡,反正你sd卡格式是fat32 的;

    正常,应当启动会有uboot打印的