This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于通过MessageQ实现核间通信的问题

Other Parts Discussed in Thread: TMS320C6678

各位大牛:

       您好,正在做一个项目,采用了TMS320C6678 芯片,使用基于MessageQ核间通信方式的双核架构,core1进行算法处理,将处理信息周期性(存在5ms周期、200ms周期和1s周期)向core0发送,core0设置专门的线程接受消息,并将收到的信息后通过以太网向外部发送,每次发送的数据量大概在400B左右。  现在出现的问题是,程序正常运行过程中,core0小概率出现核间消息接收线程卡死;当调低core1消息发送时间间隔,core0卡死的概率会增大。

     请问:(1)在什么情况下核间通信会卡死?

                (2)核间通信响应时间有没有一个上下限?下限可以测,但上限如何测?在什么文件中可以查到?间隔时间设置多少能够保证100%不会被卡死?