我看手册看到3352好像只比3359少了图形加速,就把现有的3359的winec7移植到了新生产的3352板卡上,源代码只对外设和NANDFLASH、RAM时序和配置做了改动,组件去掉了PowerVR,但是在测试过程中发现3352的板卡(5、6块)有死机的现象,不知道这样直接把bsp套用过来有问题吗?可以这样使用吗?现在暂时还没排查出是硬件问题还是软件问题,特此问一下这种移植是否可行
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
RAM是DDR3,RAM这部分本来是参考开发板,但是硬件同事说开发板的不符合DDR规范改进了下,另外PCB布局也有变化所以RAM的参数利用TI的gel改了,外设只删除没有增加,去掉了相应的组件
一开始怀疑是RAM问题,把参数重新调了下,然后利用TI的gel测试(强度比较轻)和自己在EBOOT下写的内存测试都没有出现内存错误,又没法认定就是RAM问题。。还怀疑是NANDFLASH的问题但是又不知道怎么确认。
现在把板子上的CPU换成了3359在winec7下测试,一个通宵了暂时没死机,不确定是不是CPU不同型号导致的啊