This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP5509A硬件设计问题



我在用5509A和FPGA设计一个电路板,我在参考其他电路图设计时遇到以下一些困惑,望解答:

1、5509A的FSX0引脚接一10K电阻,电阻再接电源3.3V,那么这个FSX0引脚被置高即不使用,对吗?

2、5509A和fpga直接的通信采用MCBSP接口,CLKR0和S10、S14、S20、S24连接,即MCBSP1、MCBSP2的CLKR、CLKX都是由MCBSP0的CLKR0提供,这样       可行吗?

3、参考其他原理图时看到,CLKR0还通过一个10K电阻连接到FPGA的普通IO上,这样设计是有其他用处吗?

4、另外可以提供关于MCBSP接口的应用资料吗?比如原理图连接或者软件编程资料

  • 1. 是的,另外需要将FSX0配置成输出管脚。可以参考下面的文档第8页。
    http://www.ti.com/lit/an/sprab14/sprab14.pdf 

    2.  可以的。

    3. 不清楚你说的什么原理图。

    4. 没有和FPGA连接的原理图。 

  • 感谢你回复!

    还有一问,请问:

    1、AIC23和5509A通过MCBSP连接时,只使用了DSP的一个时钟脚“CLKR0”,这个时钟脚只是MCBSP的接收时钟,为什么就不再使用CLKX0了?为什么就不需要给AIC23提供CLKX0这个MCBSP发送时钟了?

    2、如果CLKR0没有和S10  S14  S20   S24连接,那么比如S10(MCBSP.CLKR)是不是也可以提供接收时钟?

  • 1. 不知道你参考的是什么原理图?TI的5509A EVM原理图是将CLKX0和CLKR0连起来后一起接到AIC23.
    http://c5000.spectrumdigital.com/dsk5509a/files/dsk5509a_TechRef.pdf

    2.可以,在MCBSP user guide里有说明,SRG的时钟源可以来自外部的CLKR, CLKX,CLKS这些管脚。

    The input clock for the sample rate generator (labeled CLKSRG in Figure 3−1)
    can be supplied by the McBSP internal input clock or by one of these external
    pins: CLKX, CLKR, or (if present) CLKS