This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAPL138 网口初始化

Other Parts Discussed in Thread: CDCE913, AM1808, TMS320C6748, OMAP-L138

你好,我使用的OMAPL138在进行网口测试时,网口不能初始化

#include "stdio.h"

#include "string.h"

#include "types.h"

#include "evmomapl138.h"

#include "evmomapl138_timer.h"

#include "ethernet_smsc.h"

#include "evmomapl138_emac.h"

#include "evmomapl138_gpio.h"

#include "evmomapl138_i2c_gpio.h"

#include "evmomapl138_cdce913.h"

//-----------------------------------------------------------------------------

// Private Defines and Macros

//-----------------------------------------------------------------------------

// mdio clock divide down value.

#define MDIO_CLK_FREQ_HZ   (2000000)

#define MDIO_CLK_DIVISOR   ((SYSCLOCK4_HZ / MDIO_CLK_FREQ_HZ) - 1)

// packet defines.

#define MAX_RX_BUFFERS     (10)

#define MIN_PACKET_SIZE    (46)

#define MAX_PACKET_SIZE    (1518)

#define PACKET_ALIGN       (18)

// rx / tx desriptor memory offsets.

#define RX_DESC_OFFSET     (0)

#define TX_DESC_OFFSET     (0x1000)

//MII pinmux

#define PINMUX_MII_REG_0         (2)

#define PINMUX_MII_MASK_0        (0xFFFFFFF0)

#define PINMUX_MII_VAL_0         (0x88888880)

#define PINMUX_MII_REG_1         (3)

#define PINMUX_MII_MASK_1        (0xFFFFFFFF)

#define PINMUX_MII_VAL_1         (0x88888888)

//RMII pinmux

#define PINMUX_RMII_REG_0        (14)

#define PINMUX_RMII_MASK_0       (0xFFFFFF00)

#define PINMUX_RMII_VAL_0        (0x88888800)

#define PINMUX_RMII_REG_1        (15)

#define PINMUX_RMII_MASK_1       (0x000000FF)

#define PINMUX_RMII_VAL_1        (0x00000080)

//MDIO pinmux

#define PINMUX_MDIO_REG          (4)

#define PINMUX_MDIO_MASK         (0x000000FF)

#define PINMUX_MDIO_VAL          (0x00000088)

//GPIO pinmux

#define PINMUX_MII_MDIO_EN_REG (6)

#define PINMUX_MII_MDIO_EN_MASK (0x000000F0)

#define PINMUX_MII_MDIO_EN_VAL (0x00000080)

//

#define EMAC_RMII_SPEED_100 (0x00008000)

//-----------------------------------------------------------------------------

// Private Static Variables

//-----------------------------------------------------------------------------

static uint8_t g_active_phy_id = 0xFF;

static volatile emac_descriptor_t *g_rx_desc = (emac_descriptor_t *)(EMAC_RAM_BASE + RX_DESC_OFFSET);

static volatile emac_descriptor_t *g_tx_desc = (emac_descriptor_t *)(EMAC_RAM_BASE + TX_DESC_OFFSET);

static volatile emac_descriptor_t *g_rx_active_head = 0;

static volatile emac_descriptor_t *g_rx_active_tail = 0;

static uint8_t g_rx_queue_active = 0;

static uint8_t g_rx_buffers[MAX_RX_BUFFERS * (MAX_PACKET_SIZE + PACKET_ALIGN)];

//-----------------------------------------------------------------------------

// Private Function Prototypes

//-----------------------------------------------------------------------------

static uint32_t initMdioPhy(void);

static uint8_t isLinkActive(uint8_t in_phy);

static uint16_t phyRegRead(uint8_t in_phy, uint8_t in_reg);

static void phyRegWrite(uint8_t in_phy, uint8_t in_reg, uint16_t in_data);

//-----------------------------------------------------------------------------

// Public Function Definitions

//-----------------------------------------------------------------------------

//-----------------------------------------------------------------------------

// \brief   initialize the EMAC and MDIO for use.

//

// \param   none.

//

// \return  uint32_t

//    ERR_NO_ERROR - everything is ok...emac ready to use.

//    ERR_INIT_FAIL - something happened during initialization.

//-----------------------------------------------------------------------------

uint32_t EMAC_init(emac_interface_e emac_interface)

{

  uint32_t rtn = 0;

  uint32_t i;

  volatile emac_descriptor_t *tmp_rx_desc;

  // reset emac module.

  EMAC->SOFTRESET = 1;

while (EMAC->SOFTRESET != 0) {}

到这一句程序一直等待,寄存器SOFTRESET显示是0,不能读1,不知道是哪里的问题?能否说明给出解决的方法,谢谢,使用的是CCS4