This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM385网口



你好,目前通过UBOOT执行PING命令,但是有个奇怪的现象,就是PING成功的时候间隔的,也就是第一次PING,显示如下:

phy info reg 0x1e addr 0 var ffff

phy info reg 0x1e addr 0 var ffff

failed to read bmcr 

ping failed.

但是第二次ping 就成功了,显示如下:

phy info reg 0x1e addr 0 var 2

phy info reg 0x1e addr 0 var a

link up on port 0,speed 100 ,full duplex

host 192.168.253.155 is alive。

第三次又和第一次一样,第4次和第二次一样,以此类推。

  • Xin Jin,

    在Linux下也是类似的情况么?

    你的网络部分在软件和硬件上和DM385 IPNC有哪些差异?

  • 内核无法启动,我通过串口把内核写入DDR,但每次都卡在Starting kernel ...,不知道为什么。我用的是DM385,UBOOT设置的参数如下:

    set ipaddr 192.168.253.144

    ;set serverip 192.168.253.131

    set ethaddr 00:0C:0C:A0:FF:FA;

    saveenv;

    setenv bootargs 'root=/dev/nfs console=ttyO0,115200n8 mem=80M rw notifyk.vpssm3_sva=0xBFD00000 nfsroot=192.168.253.131:

    /opt/Source/ipnc_rdk/target/filesys,nolock,tcp ip=dhcp eth=$(ethaddr) cmemk.phys_start=0x85000000 cmemk.phys_end=0x89000000 cmemk.allowOverlap=1 earlyprintk';saveenv