This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168和tlv320aic301 的问题

Other Parts Discussed in Thread: TLV320AIC3101

各位前辈好,

现在我想通过DM8168的I2S口输出音频给tlv320aic301,然后通过LEFT_LO和RIGHT_LO输出。

说明:

1,sdk版本是DVRRDK_04.00.00.03

2,tlv320aic301的I2S设置为master模式,线性音频可以通过tlv320aic301输出给dm8168和LEFT_LO和RIGHT_LO。

现在关于tlv320aic301不能接受到dm8186的I2S音频然后从LEFT_LO输出,我有几个疑问?

1,tlv320aic301的I2S模式是否要设置为slave模式?

2,SW-D1,SW-D2,SW-D3,SW-D4这几个开关在哪个寄存器里面可以配置?查看了寄存器,没有找到。

3,DINL和DINR后面的进Effects之前的mux开关怎样选通?查看了寄存器,没有找到。

谢谢大家!